{"id":9074,"date":"2014-03-18T08:07:59","date_gmt":"2014-03-18T15:07:59","guid":{"rendered":"https:\/\/blogs.plm.automation.siemens.com\/t5\/Solid-Edge-Blog\/Solid-Edge-Sensors-Orifice-Plate-by-Tushar-Suradkar\/ba-p\/25174"},"modified":"2026-03-26T07:27:21","modified_gmt":"2026-03-26T11:27:21","slug":"solid-edge-sensors-orifice-plate-by-tushar-suradkar","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/solidedge\/solid-edge-sensors-orifice-plate-by-tushar-suradkar\/","title":{"rendered":"Solid Edge Sensors: Orifice Plate, by Tushar Suradkar"},"content":{"rendered":"<p><P><STRONG><BR \/><\/STRONG><EM>[editor] This is an article submitted by Tushar Suradkar for publishing in the Solid Edge Community Blog. <\/EM><\/P><\/p>\n<p><P><STRONG>Solid Edge Can Sense<\/STRONG><BR \/> <BR \/> Solid Edge has a feature called <STRONG>Sensors<\/STRONG> &#8211; call it your sixth sense.<\/P><br \/>\n<P><BR \/> And it helps everyone who uses Solid Edge &#8211; machinists, mold tooling designers, sheet metal specialists and everyone.<\/P><br \/>\n<P><BR \/> Sensors in Solid Edge are highly developed, each intended to be used for a different purpose. <BR \/> This article takes the example of an <STRONG>orifice<\/STRONG> design and shows how the <STRONG>Surface Area Sensor<\/STRONG> can make life easier for a designer.<\/P><\/p>\n<p><P><STRONG><span class=\"lia-inline-image-display-wrapper lia-image-align-right\" style=\"width: 240px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/1-14.jpg\" alt=\"1.jpg\" title=\"1.jpg\" \/><\/span>Problem Definition<\/STRONG><BR \/> <BR \/> The task is to design an orifice plate as shown in figure. The plate is circular and has numerous circular holes.<\/P><\/p>\n<p><P>Take a simplified design by using a pattern of holes along the periphery as shown in figure for next step.<\/P><\/p>\n<p><P>The <STRONG>amount <\/STRONG>or<STRONG> rate<\/STRONG> of fluid flowing through the orifice is an in-direct function of the <STRONG>surface area<\/STRONG> of the circular face of the Orifice Plate. The more the area of the face, lesser the area of the holes and lesser the amount of flowing fluid.<BR \/><STRONG>&nbsp;<\/STRONG><\/P><br \/>\n<P><STRONG><span class=\"lia-inline-image-display-wrapper lia-image-align-right\" style=\"width: 240px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/2-1.gif\" alt=\"2.gif\" title=\"2.gif\" \/><\/span><\/STRONG><STRONG>What is a Sensor<\/STRONG><BR \/> <BR \/> Keeping that in mind, setup a <STRONG>Surface Area Sensor<\/STRONG> that will alert you whenever the surface area crosses a pre-defined limit.<\/P><br \/>\n<P><BR \/> By now you must have gathered a faint idea about a sensor. Per Solid Edge Help, <BR \/> <EM>You can use the Sensors tab on the EdgeBar tool to define and keep track of design parameters for your parts and assemblies.<\/EM><\/P><\/p>\n<p><P><STRONG>Setup the Sensor<\/STRONG><BR \/> <BR \/> <STRONG><span class=\"lia-inline-image-display-wrapper lia-image-align-right\" style=\"width: 287px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/3-43.png\" alt=\"3.png\" title=\"3.png\" \/><\/span><\/STRONG>1. Click on the Sensors tab on the EdgeBar. <BR \/> see figure. <BR \/> 2. Click the <STRONG>Surface Area Sensor<\/STRONG> button at the top of this tab.<\/P><\/p>\n<p><P><STRONG>Specify Surface Areas<\/STRONG><BR \/> <BR \/> Select the top face of the Orifice Plate. <BR \/> See figure. This is the positive area.<\/P><br \/>\n<P><BR \/> Click accept<\/P><\/p>\n<p><P><span class=\"lia-inline-image-display-wrapper lia-image-align-right\" style=\"width: 236px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/5-30.png\" alt=\"5.png\" title=\"5.png\" \/><\/span>The next tool on the ribbon bar is to select negative area. Since the holes are also a part of the circular face of the plate, there is no need to specify negative area separately.<\/P><br \/>\n<P>You specify a negative area exclusively in cases where there is a disjoint area on another face on the model that you want to include in the calculations, if required by that particular design.<BR \/><STRONG>&nbsp;<\/STRONG><\/P><br \/>\n<P><STRONG>Specify Sensor Parameters<\/STRONG><BR \/> <span class=\"lia-inline-image-display-wrapper lia-image-align-inline\" style=\"width: 508px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/4-31.png\" alt=\"4.png\" title=\"4.png\" \/><\/span><BR \/> By now, the <STRONG>Sensor Parameters<\/STRONG> dialog has popped up so you can educate the sensor.<\/P><\/p>\n<p><P>Type in a <STRONG>Name<\/STRONG> for the sensor something like <STRONG>Orifice Design<\/STRONG> or even your pet&#8217;s name will do. <BR \/> In the <STRONG>Sensor Definition<\/STRONG> area, the current value is now displayed.<\/P><br \/>\n<P>Just right to the current value is the <STRONG>Edit Area Value<\/STRONG> button (<STRONG>1<\/STRONG> in fig) that you can click if you want to re-specify the area again<STRONG>.<\/STRONG><\/P><\/p>\n<p><P><STRONG>Specify Limits<\/STRONG><BR \/> <BR \/> Set other options as shown (<STRONG>2<\/STRONG> and <STRONG>3<\/STRONG> in figure) <BR \/> Specify a <STRONG>Threshold<\/STRONG> value of 1500 or as may be in your case. <BR \/> See red ball no. <STRONG>4<\/STRONG> in figure above.<\/P><br \/>\n<P><BR \/> Take a glance at the description <STRONG>generated<\/STRONG> and appreciate how the sensor also <STRONG>thinks for you<\/STRONG>. <BR \/> By setting <STRONG>Display Type<\/STRONG> to Horizontal range, you can check if the area falls between two values that you specify in the <STRONG>Sensor Range<\/STRONG> area.<\/P><br \/>\n<P><BR \/> For the present case, select <STRONG>True\/False<\/STRONG> since we are interested in checking the surface area and arrest the design when it goes beyond\/falls below a preset mark.<\/P><\/p>\n<p><P><STRONG>Sensor Ready &#8211; Test It<\/STRONG><BR \/> <BR \/> The final step is to use your sixth sense &#8211; the Orifice Sensor. <BR \/> Right click on the Sensor tab and select <STRONG>Tear Off<\/STRONG> from the menu.<\/P><br \/>\n<P><BR \/> You do this to view both the sensor and the Feature Pathfinder tab as you change the surface area.<\/P><\/p>\n<p><P><STRONG>Sensor Working<\/STRONG><BR \/> <BR \/> <span class=\"lia-inline-image-display-wrapper lia-image-align-right\" style=\"width: 265px;\"><img decoding=\"async\" src=\"http:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/0001-4.png\" alt=\"0001.png\" title=\"0001.png\" \/><\/span>Switch to the <STRONG>Feature Pathfinder<\/STRONG> tab and change the diameter of the hole or the count in the pattern (since the diameter of the plate is to be kept fixed).<\/P><br \/>\n<P>Now with the sensor <STRONG>thinking for you<\/STRONG> in the background, feel free to experiment with the orifice dimensions. <BR \/> As soon as the surface area for the Orifice Plate crosses the threshold limit that you specified earlier, the sensor will change the green signal to red.<\/P><br \/>\n<P><STRONG>Note :<\/STRONG> Anytime you wish to change any of the sensor settings, right-click on the Orifice Sensor and select <STRONG>Edit<\/STRONG> from the menu.<\/P><\/p>\n<p><P>~ Tushar Suradkar<\/P><\/p>\n","protected":false},"excerpt":{"rendered":"<p>[editor] This is an article submitted by Tushar Suradkar for publishing in the Solid Edge Community Blog.  <\/p>\n<p> Solid Edge Can Sense      Solid Edge has a feature called Sensors &#8211; call it your &#8230;<\/p>\n","protected":false},"author":61781,"featured_media":9094,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[179,1,96],"tags":[],"industry":[],"product":[],"coauthors":[],"class_list":["post-9074","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-customer-success-story","category-news","category-tips-tricks"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/8\/2019\/09\/0001-4.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/posts\/9074","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/users\/61781"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/comments?post=9074"}],"version-history":[{"count":8,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/posts\/9074\/revisions"}],"predecessor-version":[{"id":9095,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/posts\/9074\/revisions\/9095"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/media\/9094"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/media?parent=9074"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/categories?post=9074"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/tags?post=9074"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/industry?post=9074"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/product?post=9074"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/solidedge\/wp-json\/wp\/v2\/coauthors?post=9074"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}