{"id":31858,"date":"2021-10-26T05:15:12","date_gmt":"2021-10-26T09:15:12","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=31858"},"modified":"2026-03-26T06:22:16","modified_gmt":"2026-03-26T10:22:16","slug":"test-autonomous-vehicles-with-custom-algorithms-in-openscenario-designed-experiments","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/test-autonomous-vehicles-with-custom-algorithms-in-openscenario-designed-experiments\/","title":{"rendered":"Test autonomous vehicles with custom algorithms in OpenSCENARIO designed experiments"},"content":{"rendered":"\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"498\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3-1024x498.png\" alt=\"Simcenter Prescan 2021.3 provides support for the External Controller Action within the OpenSCENARIO engine\" class=\"wp-image-31859\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3-1024x498.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3-600x292.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3-768x373.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3-900x438.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3.png 1086w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption>Simcenter Prescan 2021.3 provides support for the External Controller Action within the OpenSCENARIO engine<\/figcaption><\/figure>\n\n\n\n<p class=\"has-large-font-size\">Siemens announces the release of Simcenter Prescan 2021.3. To better test autonomous vehicles, this release introduces External Controller support for OpenSCENARIO experiments, Illuminance sensor output for the Unreal Physics-based Camera and FMU support for the Prescan NI Veristand RT target, as well as many other important improvements that will help users improve the accuracy and ease-of-use of AV\/ADAS simulations.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>External Controller support<\/strong><\/h3>\n\n\n\n<p>Simcenter Prescan 2021.3 introduces the concept of the External Controller within the Open Scenario Engine which empowers users to include their custom algorithms within the Open Scenario Framework for test and validation. The user can now import an OpenSCENARIO file, connect the custom algorithm to the experiment and then the Open Scenario Engine will switch to the algorithm once a user-defined condition is satisfied. This simplifies the testing setup and the user can now use third parties OpenSCENARIO databases to test algorithms.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Illuminance sensor output for Unreal PBC<\/strong><\/h3>\n\n\n\n<p>With this release, Physics-based camera users can output the amount of light that hits visible objects, using the new Illuminance sensor. The output, provided in Lux, can be used as a ground-truth channel for algorithm accuracy and performance tests.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Materials<\/strong><\/h3>\n\n\n\n<p>Material changes are now visible in the WorldViewer and Unreal Physics-based camera. Additionally, two new materials have been added to the material library, and custom material options are available for several new objects.<\/p>\n\n\n\n<figure class=\"wp-block-image size-full\"><img loading=\"lazy\" decoding=\"async\" width=\"973\" height=\"255\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Materials-and-options.png\" alt=\"New materials and options\" class=\"wp-image-31861\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Materials-and-options.png 973w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Materials-and-options-600x157.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Materials-and-options-768x201.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Materials-and-options-900x236.png 900w\" sizes=\"auto, (max-width: 973px) 100vw, 973px\" \/><figcaption>New materials and options<\/figcaption><\/figure>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>FMU support for Prescan NI Veristand RT Target<\/strong><\/h3>\n\n\n\n<p>Simcenter Prescan 2021.3 enables the customers the use of FMI\/FMU directly within the NI RT Platform. Customers are now able to integrate their custom code or vehicle dynamics modules within Prescan, using the FMI \/ FMU format, and deploy their models with custom FMUs to the Prescan NI RT Target. This is an extension to the already exisiting FMI \/ FMU support on Prescan Desktop, and enables the user to easily make the transition from Model-in-the-Loop (MiL) simulation to Hardware-in-the-Loop (HiL) simulation for the testing &amp; validation of autonomous vehicles.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Improvements to OpenDRIVE import pipeline<\/strong><\/h3>\n\n\n\n<p>In this release GUI editable roads may be modified using the Data Model API which further enables to customers to add variations to their test scenarios via scripting.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>New Simcenter Prescan assets<\/strong><\/h3>\n\n\n\n<p>Simcenter Prescan introduces several new assets in this release. Several small target objects (cinder block, tire, shopping cart, block pallet) have been added to provide additional variation for perception and algorithm performance and accuracy testing. Furthermore, the HOWO T5G Cement truck has been added to the Prescan vehicle library. The cement truck is placed under the new \u201cHeavy Machinery\u201d tab in the GUI.<\/p>\n\n\n\n<figure class=\"wp-block-image size-full\"><img loading=\"lazy\" decoding=\"async\" width=\"976\" height=\"271\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/New-assets.png\" alt=\"New assets\" class=\"wp-image-31862\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/New-assets.png 976w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/New-assets-600x167.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/New-assets-768x213.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/New-assets-900x250.png 900w\" sizes=\"auto, (max-width: 976px) 100vw, 976px\" \/><figcaption>New assets<\/figcaption><\/figure>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Physics-based Lidar updates<\/strong><\/h3>\n\n\n\n<p>With this new release, the Point-cloud Lidar (Physics-based Lidar) supports simulation of animated pedestrians. Furthermore, experiments with this sensor can now be simulated on Linux systems.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Want more information?<\/h3>\n\n\n\n<p>Interested in the new Simcenter Prescan 2021.3 release or to better test autonomous vehicles?<\/p>\n\n\n\n<p class=\"has-large-font-size\">&nbsp;<a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/contact-us.html\" target=\"_blank\" rel=\"noopener\">You can contact us here<\/a>.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Siemens announces the release of Simcenter Prescan 2021.3. To better test autonomous vehicles, this release introduces External Controller support for&#8230;<\/p>\n","protected":false},"author":17049,"featured_media":31859,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1,179],"tags":[670,669,701,17722,629,569,216,244,219,220,26,10826],"industry":[89,132,133,134],"product":[511],"coauthors":[778],"class_list":["post-31858","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","category-product-updates","tag-adas-data-collection","tag-adas-testing","tag-artificial-intelligence","tag-automotive","tag-automotive-oems","tag-autonomous-vehicles","tag-cloud","tag-design-exploration","tag-digital-transformation","tag-digitalization","tag-engineering-services","tag-news","industry-automotive-transportation","industry-automotive-oems","industry-automotive-suppliers","industry-trucks-buses-specialty-vehicles","product-simcenter-prescan"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/10\/Prescan-2021.3.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/31858","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/17049"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=31858"}],"version-history":[{"count":4,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/31858\/revisions"}],"predecessor-version":[{"id":32084,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/31858\/revisions\/32084"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/31859"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=31858"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=31858"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=31858"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=31858"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=31858"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=31858"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}