{"id":30118,"date":"2021-08-25T09:23:54","date_gmt":"2021-08-25T13:23:54","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=30118"},"modified":"2026-03-26T06:47:16","modified_gmt":"2026-03-26T10:47:16","slug":"the-thermal-benefits-of-vapor-chambers","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/the-thermal-benefits-of-vapor-chambers\/","title":{"rendered":"The Thermal Benefits of Vapor Chambers"},"content":{"rendered":"\n<p>Vapor chambers are becoming an increasingly common thermal solution for electronic devices. They can be found in a range of systems, from mobile phones to high-powered laptops and video game consoles. In this blog we will discover what exactly is a vapor chamber; learn how to model them using CFD software; and analyze the thermal benefits of vapor chambers compared to traditional heat sinks.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">What is a vapor chamber?<\/h2>\n\n\n\n<p>A typical vapor chamber consists of a hollow copper enclosure (the chamber) that is filled with a small amount of liquid water. This chamber is then vacuum sealed below atmospheric pressure; allowing the liquid water to evaporate (the vapor) at temperatures lower than 100 \u00b0C.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"188\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-1024x188.png\" alt=\"Typical structure of a vapor chamber\" class=\"wp-image-30121\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-1024x188.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-600x110.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-768x141.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-1536x282.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-2048x376.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-Structure-900x165.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Typical structure of a vapor chamber<\/figcaption><\/figure><\/div>\n\n\n<p>The working principle behind a vapor chamber is the same as a typical heat pipe. It relies on the evaporation and condensation cycle of the water to transfer heat from the hot side of the chamber to the cooler side. The inner wick then acts as a carrier for the condensed liquid water to flow back around to the evaporation side using capillary action. Then the cycle can begin again.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"246\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-1024x246.png\" alt=\"Operating cycle of a vapor chamber\" class=\"wp-image-30122\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-1024x246.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-600x144.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-768x185.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-1536x369.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-2048x492.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Operating-Cycle-annotated-ver2-900x216.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Operating cycle of a vapor chamber<\/figcaption><\/figure><\/div>\n\n\n<p>Vapor chambers can be used as a thermal cooling solution on their own to spread and dissipate heat. This is often seen in some mobile phones where space is limited. However, vapor chambers can also be attached to the base of a conventional heatsink when even greater cooling efficiency is required.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Is a vapor chamber better than heat pipes?<\/h2>\n\n\n\n<p>Although the operating cycle for both a vapor chamber and heat pipe are similar, the choice of cooling solution will depend on the application. For instance, vapor chambers are very effective at uniformly spreading heat laterally across a surface. In contrast, heat pipes are good at transferring heat from one place to another.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"577\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-1024x577.png\" alt=\"Vapor chamber vs heat pipes\" class=\"wp-image-30222\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-1024x577.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-600x338.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-768x433.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-1536x866.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-2048x1154.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapor-Chamber-vs-Heat-Pipe-900x507.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Vapor chamber vs heat pipes<\/figcaption><\/figure><\/div>\n\n\n<p>The flat shape of a vapor chamber also means they can make better surface contact with IC chips, or to the base of an attached heat sink, to create a more direct heat transfer path. This contrasts with the cylindrical shape of a heat pipe, which prevents it being directly attached to a component. Instead they require additional connecting parts or modifications before the heat can even reach the pipes.<\/p>\n\n\n\n<p>Modern manufacturing can produce vapor chambers as thin as 2.5mm.  This makes them very useful in compact electronic devices such as mobile phones or vapor chamber laptops. In addition, their thin shape means they are less affected by orientation, unlike a traditional heat pipe where the direction of gravity can affect its cooling efficiency.<\/p>\n\n\n\n<p>In order to visualise the thermal benefits of vapor chambers, CFD analysis is performed using Simcenter Flotherm XT and this type of analysis is also be possible using <a href=\"https:\/\/plm.sw.siemens.com\/en-US\/simcenter\/fluids-thermal-simulation\/floefd\/\" target=\"_blank\" rel=\"noreferrer noopener\">Simcenter FLOEF<\/a>D, CAD embedded CFD software.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Modeling a vapor chamber in a CFD simulation tool<\/h2>\n\n\n\n<p>Let\u2019s start by taking a typical model of a high-powered video game console. Most of the heat output is from the main System on a Chip (SoC) producing 100 watts of thermal power. We will compare the SoC temperatures with 2 different attached heat sinks: First a standard copper base heat sink, then with a vapor chamber base heat sink. Both will be of equal size and with aluminium plane fins attached.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"735\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-1024x735.png\" alt=\"Model used for heat sink comparison \" class=\"wp-image-30125\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-1024x735.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-600x431.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-768x551.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-1536x1102.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model-900x646.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Base-Model.png 1983w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Model used for heat sink comparison<\/figcaption><\/figure><\/div>\n\n\n<p>Modelling a vapor chamber explicitly is not a straightforward endeavour. It requires a lot of computational time (and an engineer\u2019s time) to model the evaporation and condensation cycle on which they operate. Because of this, it is often quicker and more convenient to create a simplified model, which will closely approximate our desired vapor chamber characteristics.<\/p>\n\n\n\n<p>We will take our standard heat sink in the model above, and modify the copper base into a sandwich of solid conduction layers that represent the vapor chamber:<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-full is-resized\"><img loading=\"lazy\" decoding=\"async\" width=\"1025\" height=\"742\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/VPR-heat-sink-cross-section-cut-ver2.png\" alt=\"Cross-section cut showing the solid material layers used to represent the vapor chamber, which is attached to the aluminium heat sink fins\" class=\"wp-image-30126\" style=\"width:513px;height:371px\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/VPR-heat-sink-cross-section-cut-ver2.png 1025w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/VPR-heat-sink-cross-section-cut-ver2-600x434.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/VPR-heat-sink-cross-section-cut-ver2-768x556.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/VPR-heat-sink-cross-section-cut-ver2-900x652.png 900w\" sizes=\"auto, (max-width: 1025px) 100vw, 1025px\" \/><figcaption class=\"wp-element-caption\">Cross-section cut showing the solid material layers used to represent the vapor chamber, which is attached to the aluminium heat sink fins<\/figcaption><\/figure><\/div>\n\n\n<p>We can now apply effective thermal conductivities to the newly added wick and water vapor layers. We will use values that best approximate the vapor chamber in its operational state:<\/p>\n\n\n\n<p class=\"has-text-align-center\">Wick = 40 W\/(m K)<\/p>\n\n\n\n<p class=\"has-text-align-center\">Water Vapor = 30 000 W\/(m K)<\/p>\n\n\n\n<p>You may notice the very high effective thermal conductivity of the water vapor. This gives us some insight into the type of cooling performance we can expect to see from our vapor chamber!<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">CFD analysis of a vapor chamber<\/h2>\n\n\n\n<p>The model was first solved using the standard copper base heat sink. This was then followed by a second solve with the vapor chamber heat sink. The forced air flow pattern through the device can be seen below:<\/p>\n\n\n\n<figure class=\"wp-block-video aligncenter\"><video autoplay controls loop muted preload=\"auto\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/air-flow-temp-Ver-2_Trim.mp4\"><\/video><\/figure>\n\n\n\n<p>By generating a temperature plane plot on the vertical axis, we can take a look at the SoC temperatures using the standard copper base heat sink:<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"424\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-1024x424.png\" alt=\"Standard copper base heat sink\" class=\"wp-image-30127\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-1024x424.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-600x248.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-768x318.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-1536x635.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-2048x847.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Standard-Copper-Results-all-in-1-900x372.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Standard copper base heat sink<\/figcaption><\/figure><\/div>\n\n\n<p>The SoC reaches a temperature of 89\u00b0C, with heat accumulation centred around the middle of the heat sink. Notice that a \u0394T of 10\u00b0C occurs from the centre to the outer edge of the copper base. This shows that the heat is unable to effectively reach the outermost fins of the attached aluminium heat sink. Consequently, this results in an inefficient use of the surrounding air flowing between the aluminium fins.<\/p>\n\n\n\n<p>Now let\u2019s take a look at the SoC temperatures using the vapor chamber heat sink:<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"428\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-1024x428.png\" alt=\"Vapor chamber heat sink CFD simulation result\" class=\"wp-image-30128\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-1024x428.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-600x251.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-768x321.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-1536x642.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-2048x856.png 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Vapour-Chamber-Results-all-in-1-900x376.png 900w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption class=\"wp-element-caption\">Vapor chamber heat sink<\/figcaption><\/figure><\/div>\n\n\n<p>This plane plot reveals a 5\u00b0C drop in temperature for the SoC compared to that of the copper base heat sink, which is an excellent improvement! In addition, the vapor chamber exhibits a \u0394T of just 3\u00b0C from the centre to the outer edge. This demonstrates a more uniform and improved lateral spreading of the SoC heat \u2013 a common benefit of using vapor chambers!<\/p>\n\n\n\n<p>As a result of the improved lateral spreading, the vapor chamber has enabled the heat to flow more evenly across a higher portion of the attached aluminium heat sink fins. Consequently, this allows better utilisation of the total volume of air flowing across all the fins. This is in contrast to the copper base heat sink, which only effectively utilised the middle fins and central air flow.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Conclusion<\/h2>\n\n\n\n<p>Modern electronic devices require more advanced cooling technology than ever before, and vapor chambers can be an excellent thermal solution. Using Simcenter CFD software tools, we have visually demonstrated the thermal benefits of vapor chambers; showing how they can offer improved cooling efficiency with better lateral heat spreading than a traditional heat sink of the same size.<\/p>\n\n\n\n<p>Have you seen any other devices or different industries utilising vapor chambers as a thermal cooling solution? If so, we would love to hear about them in the comments section below!<\/p>\n\n\n\n<hr class=\"wp-block-separator has-css-opacity is-style-wide\"\/>\n\n\n\n<h3 class=\"wp-block-heading\">Further reading:<\/h3>\n\n\n\n<ul class=\"wp-block-list\">\n<li><a href=\"https:\/\/celsiainc.com\/heat-sink-blog\/vapor-chamber-cooling-design\/\" target=\"_blank\" rel=\"noreferrer noopener\">Celsia &#8211; Vapor Chamber Cooling Design Guide<\/a><\/li>\n\n\n\n<li><a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/are-heat-pipes-any-good-for-my-cpu\/\" target=\"_blank\" rel=\"noreferrer noopener\">Are heat pipes any good for my CPU?<\/a><\/li>\n<\/ul>\n","protected":false},"excerpt":{"rendered":"<p>Learn about the thermal benefits of vapor chambers and discover why they are such an effective cooling solution for modern electronic devices.<\/p>\n","protected":false},"author":78113,"featured_media":30120,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1,182],"tags":[5,10827,662,242,243,244,10824,10822,649],"industry":[146,145],"product":[500,503,505],"coauthors":[14684],"class_list":["post-30118","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","category-tips-tricks","tag-cae-simulation","tag-cfd","tag-cfd-for-engineers","tag-computational-fluid-dynamics-cfd","tag-computer-aided-engineering-cae","tag-design-exploration","tag-electronics-semiconductors","tag-electronics-cooling","tag-fluid-analysis","industry-consumer-industrial-electronics","industry-electronics-semiconductors","product-simcenter-floefd","product-simcenter-flotherm","product-simcenter-flotherm-xt"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2021\/08\/Main-Display-Image.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/30118","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/78113"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=30118"}],"version-history":[{"count":4,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/30118\/revisions"}],"predecessor-version":[{"id":68130,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/30118\/revisions\/68130"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/30120"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=30118"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=30118"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=30118"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=30118"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=30118"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=30118"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}