{"id":15444,"date":"2020-06-03T06:46:11","date_gmt":"2020-06-03T10:46:11","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=15444"},"modified":"2026-03-26T06:08:42","modified_gmt":"2026-03-26T10:08:42","slug":"hardware-in-the-loop-solution-with-national-instruments-real-time-controllers","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/hardware-in-the-loop-solution-with-national-instruments-real-time-controllers\/","title":{"rendered":"Prescan 2020.2 release presents a new hardware-in-the-loop solution compatible with NI hardware"},"content":{"rendered":"\n<p><\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"576\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-1024x576.png\" alt=\"Test real ECU\u2019s with simulated data in real-time with this hardware-in-the-loop solution with National Instruments real-time controllers.\" class=\"wp-image-15446\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-1024x576.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-600x338.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-768x432.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-1536x864.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1-1110x624.png 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1.png 1920w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption><br>Test real ECU\u2019s with simulated data in real-time<\/figcaption><\/figure>\n\n\n\n<p class=\"has-medium-font-size\">Simcenter Prescan, the best physics-based simulation platform for testing and development of automated vehicles, announces the release of version 2020.2. This release introduces the hardware-in-the-loop simulations with National Instruments Hardware. Including the annotation tool for the Simcenter Prescan viewers, the expansion of the OpenSCENARIO importer features as well as a Beta version of the OpenSCENARIO API.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Hardware-in-the-loop simulations with National Instruments Hardware<\/strong><\/h3>\n\n\n\n<p>With release 2020.2, Prescan introduces the capability to execute a full simulation from a National Instruments PXI Controller. This means that users now can now compile a Prescan experiment, and run it within National Instruments\u2019 hardware in a hardware-in-the-loop solution. Simultaneously  ensuring their simulation is executed in hard real-time. This solution enables Simcenter Prescan users to test their ECU\u2019s with the best-in-class sensor data provided by Simcenter Prescan. The new National Instruments hardware-in-the-loop solution ensures the continuity of the simulation assets and experiments all through the lifecycle. From Software in the Loop, to Hardware in the Loop, enhancing the Time To Market of new ADAS and AV functionality.  That counts for AEBS systems as well as functionality.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>New Prescan viewer &amp; annotation capabilties<\/strong><\/h3>\n\n\n\n<p>A new viewer is also introduced, allowing users to easily generate screen annotations. It also allows users to easily add text, lines, and other shapes to highlight important content in a demonstrator system. The annotations can be setup easily via the Prescan Data Model API. They can be updated in runtime to provide close loop feedback of important information. For example: speed and acceleration of a vehicle. The picture shown in this blog post showcases how the new annotation system is used to visualize the performance of multiple ADAS systems in simulation.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>New OpenSCENARIO importer features and OpenSCENARIO API<\/strong><\/h3>\n\n\n\n<p>Prescan 2020.2 expands the OpenSCENARIO importer features, which now include support for relative conditions, like relative distance. Additionally, a Beta version of the OpenSCENARIO API has been released. This allows users to experiment with the modification of experiment created by importing OpenSCENARIO files. In subsequent releases, this API will be expanded to allow users to create event-based scenarios without need for importing any file.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>New Ground Truth Lane Marker Sensor<\/strong><\/h3>\n\n\n\n<p>The new Lane Marker sensor enabled users to verify and validate Lane Keeping Assistant and Path tracking and Following applications in seamless way. This is a result of enhanced execution performance, the data processing and the expandability of this new Ground Truth sensor.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Traffic light synchronization between Prescan and Aimsun Next<\/strong><\/h3>\n\n\n\n<p>With this new release it is possible to synchronize traffic lights from Aimsun Next to Prescan. The traffic lights which are designated to be used in this way, will be controlled by Aimsun Next, while at the same time being visualized in Prescan. The demo of the Aimsun plugin, included in the Prescan installation, shows an example of the use of this new feature.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Introduction of a wide range of GPS projections, including UTM<\/strong><\/h3>\n\n\n\n<p>In Prescan 2020.2 a wide range of GPS projections can be used, including UTM. This allows for more extensive world modeling and a more precise import of GPS signals and OpenDRIVE maps. It also extends the options for connecting to third party tools. The new GPS system is based on Proj4, and the projections are defined by specific projection strings.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Several new features for OpenDRIVE and DMAPI created roads<\/strong><\/h3>\n\n\n\n<p>Several new features have been added for OpenDRIVE and Data Model API created roads. The gaps that could be visible on junctions of OpenDRIVE imported road networks can now be filled via the Data Model API. Next to that, it is now possible to create embankment and change the lane types for OpenDRIVE roads and roads created with the Data Model API.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong><strong>Other updates<\/strong><\/strong><\/h3>\n\n\n\n<p>The GIDAS plugin has been updated to support the latest GIDAS standard, PCM v5.0. Other than that, BSM, CAM and DENM message types of the V2X plugin have been updated to the latest ASN.1 specifications.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\"><strong>Want more information?<\/strong><\/h3>\n\n\n\n<p>Interested in the new Simcenter Prescan 2020.2 release, including the hardware- in-the-loop simulations with National Instruments hardware? <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/contact-us.html\" target=\"_blank\" rel=\"noopener\">You can contact us here<\/a>.<\/p>\n\n\n\n<p>For more general information about Simcenter Prescan, <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/simulation-test\/active-safety-system-simulation.html\" target=\"_blank\" rel=\"noopener\">visit our webpage<\/a> or <a href=\"https:\/\/www.plm.automation.siemens.com\/media\/global\/en\/Siemens%20PLM%20Simcenter%20PreScan%20fs_tcm27-70172.pdf\" target=\"_blank\" rel=\"noopener\">download the Simcenter prescan fact sheet<\/a>.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Simcenter Prescan, the best physics-based simulation platform for testing and development of automated vehicles, announces the release of version 2020.2. This release introduces the Hardware in the Loop simulations with National Instruments Hardware<\/p>\n","protected":false},"author":17049,"featured_media":15446,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[331,629,639,569,2,627,86,16],"industry":[132,133,135,134],"product":[511],"coauthors":[],"class_list":["post-15444","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","tag-wheretodaymeetstomorrow","tag-automotive-oems","tag-automotive-suppliers","tag-autonomous-vehicles","tag-product-launches","tag-simcenter-engineering","tag-simulation","tag-system-simulation","industry-automotive-oems","industry-automotive-suppliers","industry-motorcycles-bicycles-parts","industry-trucks-buses-specialty-vehicles","product-simcenter-prescan"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/06\/AEB_Midday-2020.2-release-1.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/15444","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/17049"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=15444"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/15444\/revisions"}],"predecessor-version":[{"id":16112,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/15444\/revisions\/16112"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/15446"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=15444"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=15444"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=15444"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=15444"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=15444"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=15444"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}