{"id":14400,"date":"2020-05-14T04:20:00","date_gmt":"2020-05-14T08:20:00","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=14400"},"modified":"2026-03-26T06:30:46","modified_gmt":"2026-03-26T10:30:46","slug":"water-cooling-in-electronics-thermal-management","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/water-cooling-in-electronics-thermal-management\/","title":{"rendered":"Using water cooling in electronics thermal management &#8211; a PC cooling example"},"content":{"rendered":"\n<p>Water Cooling? Sounds intriguing, but can liquid cooling be an effective method for thermal management of a PC system? Short answer = Yes and below I explore this topic using simulation to illustrate how.<\/p>\n\n\n\n<p>I created this water-cooled PC&nbsp;model based on what is typically available on the current market. The water cooling system design was incorporated such that there was sufficient contact between the cooling plate and the CPU, without the tubes obstructing the RAM slots adjacent to the CPU. A radiator was attached to the roof vent in the case and connected to the pipes. A flow device was used to replicate a pump forcing fluid flow through the closed loop system. The idea being, heat would be transferred from the CPU to the water via conduction which would travel up to the radiator, and transfer heat between air gaps within the radiator, allowing heat dissipation to the surroundings. A fluid subdomain was used to assign the coolant fluid of water inside the system.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">How good is the current water cooled PC system?<\/h2>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-1.png\" alt=\"Water cooled PC - an initial plane plot view illustrating the maximum simulation temperature in the CPU die\" class=\"wp-image-14403\" width=\"577\" height=\"432\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-1.png 903w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-1-600x450.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-1-768x576.png 768w\" sizes=\"auto, (max-width: 577px) 100vw, 577px\" \/><figcaption class=\"wp-element-caption\">Plane Plot View illustrating the maximum simulation temperature in the CPU die<\/figcaption><\/figure><\/div>\n\n\n<p>I wanted to have an idea of how the current water cooling method would behave and decided to test its effectiveness in a CFD simulation with the same input parameters as seen in the past blogs. CPU temperature = 72 deg C!! This was worse than the stock cooler in <strong>blog 3<\/strong> <a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/utilizing-cfd-to-analyse-a-pc-cooling-system\/\">[Utilizing CFD to <\/a><a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/utilizing-cfd-to-analyse-a-pc-cooling-system\/\" target=\"_blank\" rel=\"noreferrer noopener\">analyse<\/a><a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/utilizing-cfd-to-analyse-a-pc-cooling-system\/\"> a PC Cooling System]<\/a>\u2026but why? Well, this was due to poor heat transfer occurring as the water was passing through the cooling block over the CPU. The plate and water did not have sufficient surface area contact to give enough time for the heat to be transferred effectively as the water flowed through the system.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">How to improve liquid cooling performance<\/h2>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"394\" height=\"565\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cool-Heatsink-cutplot.png\" alt=\"Water cooling: Liquid cooled Heat Sink design - PC liquid cooling CFD simulation model\" class=\"wp-image-14404\"\/><figcaption class=\"wp-element-caption\">Overview of Heat Sink<\/figcaption><\/figure><\/div>\n\n\n<p>Add a heat sink. We have already seen the effectiveness of heat sinks in transferring heat in Blog 3. Adding a heat sink would increase the surface area contact with the water cooling fluid flow, as well as slightly impeding the flow allowing enough time for the heat to be transferred to the water.<\/p>\n\n\n\n<p>A key project aim was to design a detailed PC water cooling system model that was simple enough to solve in a timely fashion. Avoiding an over defined mesh when adding small details and geometric complexity to areas of a model, such as adding this small heat sink to the CPU, is always important in CFD simulation. I used regions to adjust the mesh parameters such that the&nbsp;solve time was suitable and provided good accuracy in results.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Liquid-Cooling-lowe-convergence.png\" alt=\"\" class=\"wp-image-14452\" width=\"445\" height=\"240\"\/><figcaption class=\"wp-element-caption\">Graph illustrating Iterations against CPU Peak Temperature<\/figcaption><\/figure><\/div>\n\n\n<p>Once this was done, it was time for another CFD simulation. CPU temperature = 55 Deg C! Here we see the improvements with the addition of a small heat sink. A huge improvement indeed. The rate of heat transfer from the radiator to the surroundings was insufficient to maintain a low water temperature. Which meant that the water was not losing heat efficiently and its temperature continued to rise over time. For this reason the peak temperature did not converge quickly during the simulation.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">How can we enhance the water cooling design even further?<\/h2>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Close-Up.png\" alt=\"Water cooling for PC cooling - an xxterior view of liquid cooling system within CFD simulation software interface\" class=\"wp-image-14405\" width=\"506\" height=\"433\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Close-Up.png 1003w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Close-Up-600x514.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Close-Up-768x658.png 768w\" sizes=\"auto, (max-width: 506px) 100vw, 506px\" \/><figcaption class=\"wp-element-caption\">Exterior view of liquid cooling system<\/figcaption><\/figure><\/div>\n\n\n<p>Add a fan to dissipate heat more efficiently to the surroundings. Again, this was explored in blog 3, increasing rate of flow and thus improving heat transfer. I decided to change the liquid cooling system fluid used to a glycol water mixture as this is typically the fluid used as coolant and it alleviates problems with water expansion damaging the pipes during colder temperatures. It was also important to consider the roughness on the surfaces of the material. The majority of the casing material was galvanized steel and so this was accounted for using the roughness feature in model data. At this point I solved the model again to see the improvement.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Final-Temp.png\" alt=\"Water cooling: Simulation of Peak CPU  Temperature for a liquid cooled PC - Simcenter Flotherm XT\" class=\"wp-image-14406\" width=\"542\" height=\"473\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Final-Temp.png 972w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Final-Temp-600x524.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Water-Cooler-Final-Temp-768x671.png 768w\" sizes=\"auto, (max-width: 542px) 100vw, 542px\" \/><figcaption class=\"wp-element-caption\">Peak CPU Simulation Temperature &#8211; Water cooling<\/figcaption><\/figure><\/div>\n\n\n<p>48 Deg C with water cooling! This is roughly a 15 deg C drop in average temperature, in comparison to the stock cooled PC model running at peak performance, which was a huge improvement and a testament to the capabilities of water cooling. In reality the power levels and ambient temperature will tend to fluctuate, so this temperature could trend up or down depending on these circumstance. However, this is a good estimate of what we could expect the typical temperature to be when running this particular PC with the designed water cooler.<\/p>\n\n\n\n<figure class=\"wp-block-video\"><video autoplay controls loop muted poster=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/WaterCoolingPCcoolingCFDsimulationLiquidCooling.png\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/PC-Water-Cooled-Fluid-Flow.mp4\"><\/video><figcaption class=\"wp-element-caption\">Water cooling: Fluid flow inside the liquid cooling system<\/figcaption><\/figure>\n\n\n\n<p>There is room for potential improvement by adjusting the flow rate of the fluid with optimization using parametric studies. It would also be interesting to note the impact of opening the case on peak temperatures.&nbsp;<\/p>\n\n\n\n<p>If you would like to know more about <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/simcenter\/flotherm-xt.html\" target=\"_blank\" rel=\"noreferrer noopener\">Simcenter Flotherm XT<\/a> for liquid or air cooled electronics design &#8211; try it out for yourself with a&nbsp;<a href=\"https:\/\/trials.sw.siemens.com\/simcenter-flotherm-xt\/\" target=\"_blank\" rel=\"noreferrer noopener\">free cloud evaluation<\/a>.&nbsp;<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><strong>Other resources: water cooling and electronics liquid cooling thermal management<\/strong><\/h2>\n\n\n\n<p>For an overview of how CFD simulation of any liquid cooling systems is applied to design of electronics such as servers for edge computing, see this <a href=\"https:\/\/www.youtube.com\/watch?v=zy6YWm8gYbU\" target=\"_blank\" rel=\"noopener\">video interview<\/a> with Iceotope Technologies.  <br><br>For industry and technical insights into liquid cooling for<strong> AI hardware <\/strong>and AI chip thermal management in particular, please this <a href=\"https:\/\/webinars.sw.siemens.com\/en-US\/ai-hardware-thermal-management-deep-learning-chip-cooling\/\" target=\"_blank\" rel=\"noreferrer noopener\">on-demand webinar<\/a> presentation on cooling of a Deep Learning Machine application with insights from Guy Wagner at Electronic Cooling Solutions Inc on a project undertaken for Cerebras.<br><br>For liquid cooling in large systems with piping and sub systems such as in data centers, some avionics  and also electric vehicle power electronic cooling systems, 1D system level modeling tools are used for speed and scale to evaluate systems.  I draw your attention to a new technology to derive fast solving, accurate <strong>reduced order thermal models<\/strong> from 3D thermal analysis models that preserves 3D conduction analysis accuracy in any thermal environment.  <br><br><strong>Simcenter Flotherm BCI-ROM<\/strong> (boundary-condition-reduced order model) technology is available in several 3D  electronics cooling CFD Simcenter tools to generate BCI-ROMs in 3 formats. The BCI-ROMs in appropriate format are valueable for transient thermal analysis in electrothermal modeling in circuit simulation tools (VHDL-AMS format)  beside thermal modeling in system simulation tools (FMU format).  The  blog below look at using BCI-ROMsgenerated in FMU format for a PCB + cold plate assembly that are then within a simple liquid cooling system model for pump performance and thermal operational evaluation studies:<br>&#8211;  <a href=\"https:\/\/blogs.sw.siemens.com\/simulating-the-real-world\/2020\/11\/03\/how-cool-is-that-a-1d3d-approach-to-simulating-liquid-cooling\/\" target=\"_blank\" rel=\"noreferrer noopener\">How Cool is that? A 1D3D Approach to Simulating Liquid Cooling <\/a><\/p>\n\n\n\n<p class=\"has-text-align-center\">.<a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/are-heat-pipes-any-good-for-my-cpu\/\">\u2190 Previous<\/a> | Next \u2192<\/p>\n","protected":false},"excerpt":{"rendered":"<p>Water Cooling? Sounds intriguing, but can liquid cooling be an effective method for thermal management of a PC system? Short&#8230;<\/p>\n","protected":false},"author":69480,"featured_media":14402,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1,182],"tags":[242,10822,633,86],"industry":[146,147,145,148,149],"product":[505],"coauthors":[18252],"class_list":["post-14400","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","category-tips-tricks","tag-computational-fluid-dynamics-cfd","tag-electronics-cooling","tag-pc-cooling","tag-simulation","industry-consumer-industrial-electronics","industry-electronic-manufacturing-services","industry-electronics-semiconductors","industry-semiconductor-devices","industry-semiconductor-equipment","product-simcenter-flotherm-xt"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/05\/Fluid-Subdomain.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/14400","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/69480"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=14400"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/14400\/revisions"}],"predecessor-version":[{"id":50809,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/14400\/revisions\/50809"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/14402"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=14400"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=14400"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=14400"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=14400"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=14400"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=14400"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}