{"id":13209,"date":"2020-05-07T07:00:45","date_gmt":"2020-05-07T11:00:45","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=13209"},"modified":"2026-03-26T06:14:35","modified_gmt":"2026-03-26T10:14:35","slug":"how-rule-of-mixtures-is-killing-your-composite-design","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/how-rule-of-mixtures-is-killing-your-composite-design\/","title":{"rendered":"How Rule of Mixtures is Killing Your Composite Design"},"content":{"rendered":"\n<p>What engineers consider to be a \u201ccomposite\u201d is always changing. Just as there is no single definition, there is also no single analytical method that can safely predict their dynamic behavior. Just as you cannot obtain ideal performance by using a single material throughout an entire car, you can\u2019t expect to use a single analytical method to predict the behavior of all composites. <\/p>\n\n\n\n<p>Rule of Mixtures is probably the most known and widespread\nmethod of estimating composite properties. Its notoriety in composite design\ncircles is also its main problem: Rule of Mixtures has been overused and\napplied to cases that do not even come close to respecting its original,\nsimplifying assumptions. If you wish to trust your analysis, it is essential to\nfind out when it is okay, and (more importantly) not okay to use Rule of\nMixtures. This article will describe what this rule really says and will show\nsome consequences of abusing this \u201crule of thumb\u201d for composite behavior. <\/p>\n\n\n\n<h2 class=\"wp-block-heading\">What is Rule of Mixtures? <\/h2>\n\n\n\n<p>The Rule of Mixtures is actually composed of two models: Voigt, W. (1889) and Reuss, A. (1929). The first model is normally applied to calculate elastic modulus on the fiber direction, while the second one is used for estimations on the transverse direction. The common assumption in both models is that a composite microstructure is approximated like this:<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"500\" height=\"222\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/04\/rule-of-mixtures-2.png\" alt=\"\" class=\"wp-image-13210\"\/><\/figure>\n\n\n\n<p>So if your composite microstructure is always exactly like\nthose two \u201cblocks,\u201d then Rule of Mixtures is a great option for you, and you\ndon\u2019t even need to bother reading the rest of this post.<\/p>\n\n\n\n<p>However, we all know most composites don\u2019t look like this.\nEven continuous fiber composites, whose properties are often estimated using\nRule of Mixtures, have a different type of microstructure. But this isn\u2019t just\nabout \u201cthe looks.\u201d The geometric assumptions affect how the local field variables\nare estimated. Therefore, using the wrong geometry, even for \u201csimilar\u201d\ncomposites such as continuous fibers, can bring errors to local stress\/strain\nfields and consequently affect their properties and failure predictions.&nbsp;<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Why doesn&#8217;t it work? <\/h2>\n\n\n\n<p><strong>It doesn\u2019t matter how sophisticated your failure model is. Your results will still be inaccurate because their inputs \u2013 the local fields \u2013 were based on incorrect initial assumptions. It is like building a fancy house on top of a weak foundation \u2013 it is a waste of time and money.&nbsp;<\/strong><\/p>\n\n\n\n<p>So let\u2019s understand the root of these inaccuracies.&nbsp;<\/p>\n\n\n\n<p>In the first model, the assumption is that under uniaxial tension, the&nbsp;strains on the fibers and resins are the&nbsp;same<strong>,&nbsp;<\/strong>while the&nbsp;stresses are&nbsp;proportional to each constituent\u2019s&nbsp;moduli<strong>.<\/strong>&nbsp;That is not quite true, but luckily, fiber mechanical properties are normally one order of magnitude larger than resin properties. Therefore, it is common for the axial direction response to be fiber-dominated with the influence of resin being quite small. Under those circumstances, the experimental results show acceptable agreement with the first model equation.&nbsp;<\/p>\n\n\n\n<p>This explains why Rule of Mixtures can still be reasonably\napplied in practice to axial response of continuous fibers despite the\ngeometric inaccuracies of the model, even for this given composite. However,\nthe bigger problem lies in the prediction of transverse direction properties,\nas we discuss below.&nbsp;<\/p>\n\n\n\n<p>In the second model, the extra assumption is reversed:\nthe&nbsp;stresses&nbsp;on the\nfibers and the resin are the&nbsp;same,&nbsp;while&nbsp;strains&nbsp;are now&nbsp;inversely proportional&nbsp;to each\nconstituent\u2019s&nbsp;moduli.\nHowever, this time you can\u2019t count luck, as this model is much more inaccurate\nthan the first one. This is partially because the fibers will \u201cprotect\u201d\nportions of the resin from stress while causing other resin areas to be\nover-stressed, as seen in the below image of the fringe patterns of microscale\nstress distribution.&nbsp;<\/p>\n\n\n\n<p>So much for equivalent stresses among constituents \u2013 the\nstresses are not constant, not even throughout the same constituent! But the\nconsequences of that go beyond simply predicting wrong moduli.&nbsp;<\/p>\n\n\n\n<p><strong>In reality, damage initiates sooner than one would predict\nby using Rule of Mixtures. Therefore, your Rule of Mixtures-based design is not\nso safe anymore.&nbsp;<\/strong><\/p>\n\n\n\n<p>So what? You can always overdesign, right? Wrong!&nbsp;<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">The problem with overdesigning<\/h2>\n\n\n\n<p>In an ever-competitive market, overdesign is each day more\nthe last resort. In fact, with tight margins and increasing competition, small\namounts of overdesign can mean the difference between winning or losing a\nclient for the competition. Sometimes, even the business feasibility of\nemploying composites at all can be compromised because of overdesign. Not\nsurprisingly, as the cost of overdesign can be quite high.&nbsp;<\/p>\n\n\n\n<p><a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/multiscale-analysis-a-general-overview-and-its-applications-in-material-design\/\">The solution to this problem isn\u2019t simply switching to a more sophisticated&nbsp;<em>analytical&nbsp;<\/em>method.<\/a> Again, composites are always changing and no single, or even a collection of, analytical methods will help predict their dynamic behavior.&nbsp;<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"250\" height=\"224\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/04\/rule-of-mixtures.jpg\" alt=\"\" class=\"wp-image-13211\"\/><\/figure>\n\n\n\n<p>The need for flexibility has never been greater. In the same way FEA has freed engineers from using the same old shapes for their products and brought flexibility to allow evaluation of designs that never existed before, this method can also be expanded to bring the same flexibility to the material level so engineers can best employ the materials of yesterday, today, and tomorrow.&nbsp;<\/p>\n\n\n\n<p>To learn how Siemens is supporting the accurate modeling and simulation of advanced materials, click <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/simcenter\/multimech.html\" target=\"_blank\" rel=\"noopener\">here<\/a>. <\/p>\n","protected":false},"excerpt":{"rendered":"<p>Rule of Mixtures is probably the most known and widespread method of estimating composite properties. Its notoriety in composite design circles is also its main problem: Rule of Mixtures has been overused and applied to cases that do not even come close to respecting its original, simplifying assumptions. <\/p>\n","protected":false},"author":69599,"featured_media":13215,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[693,5,695,243,251,694],"industry":[],"product":[577],"coauthors":[],"class_list":["post-13209","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","tag-advanced-materials","tag-cae-simulation","tag-composites","tag-computer-aided-engineering-cae","tag-finite-element-analysis","tag-materials-engineering","product-simcenter-3d"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/04\/Rule-of-Mixtures-Featured.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/13209","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/69599"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=13209"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/13209\/revisions"}],"predecessor-version":[{"id":22607,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/13209\/revisions\/22607"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/13215"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=13209"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=13209"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=13209"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=13209"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=13209"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=13209"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}