{"id":10894,"date":"2020-02-25T07:02:17","date_gmt":"2020-02-25T12:02:17","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/simcenter\/?p=10894"},"modified":"2026-03-26T06:29:22","modified_gmt":"2026-03-26T10:29:22","slug":"creating-a-cpu-from-scratch","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/simcenter\/creating-a-cpu-from-scratch\/","title":{"rendered":"Creating a CPU thermal model from scratch quickly"},"content":{"rendered":"\n<p class=\"has-text-align-center has-cyan-bluish-gray-color has-text-color\">CPU created in Simcenter Flotherm Package Creator<\/p>\n\n\n\n<p>The most important component within a typical PC computer is the CPU. So when it comes to creating a CFD model of a computer, correctly modelling the CPU is priority number one. <\/p>\n\n\n\n<p>You could just take the easy route and create a block of the\nsame size and material and throw it into your model and solve. Which is exactly\nwhat I did to start.<\/p>\n\n\n\n<p>I had the dimensions of the CPU and created a simple component in EDA Bridge within Simcenter Flotherm XT. A power was added and the material was set to silicon as that was the material of the die. Surely this will give results close enough while keeping mesh count down?<\/p>\n\n\n\n<p>It will to some extent. However, a CPU is not only made of silicon. There is the substrate, solder and many more materials, which all have different thermal properties meaning the heat spreading within and heat transfer through the component and board will be different between a single block and a real CPU.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\">So how do you create a CPU package thermal model? <\/h2>\n\n\n\n<p>With the newly-released  Simcenter Flotherm Package Creator engineers can quickly generate clean CAD geometry based, detailed chip package models. This helped me create a very accurate model of a CPU in a matter of minutes. It would otherwise have days of effort to create in a CAD program. The only thing I needed was some dimensions about the Intel i5 chip I was modelling.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls-1022x1024.jpg\" alt=\"\" class=\"wp-image-10945\" width=\"407\" height=\"408\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls-1022x1024.jpg 1022w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls-600x600.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls-150x150.jpg 150w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls-768x769.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/solder-balls.jpg 1053w\" sizes=\"auto, (max-width: 407px) 100vw, 407px\" \/><figcaption class=\"wp-element-caption\">Underside of CPU model with detailed solder balls<\/figcaption><\/figure><\/div>\n\n\n<p>While this was detailed, it created its own problem. The solder balls were so small that it caused the mesh count to be over 1 million! To avoid overly long solve times at this early stage of design evaluation,  I decided to model the solder as a compact model which is still quite accurate as it uses an orthotropic conductivity for the solder ball region. This reduced the mesh count to less than 200,000 and saved me over an hour in solve time.<\/p>\n\n\n<div class=\"wp-block-image\">\n<figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder-1024x1021.jpg\" alt=\"\" class=\"wp-image-10944\" width=\"442\" height=\"440\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder-1024x1021.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder-600x598.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder-150x150.jpg 150w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder-768x766.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/compact-solder.jpg 1053w\" sizes=\"auto, (max-width: 442px) 100vw, 442px\" \/><figcaption class=\"wp-element-caption\">Compact solder modelling which reduced mesh count massively<\/figcaption><\/figure><\/div>\n\n\n<p>It was easy to export the package and use EDA Bridge to replace the simple component and create some interesting results on a motherboard. These were close to the results seen in the previous blog post.<\/p>\n\n\n\n<figure class=\"wp-block-gallery aligncenter has-nested-images columns-default is-cropped wp-block-gallery-1 is-layout-flex wp-block-gallery-is-layout-flex\">\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"740\" data-id=\"10939\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-1024x740.jpg\" alt=\"\" class=\"wp-image-10939\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-1024x740.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-600x434.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-768x555.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-1536x1110.jpg 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result-1110x802.jpg 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/top-result.jpg 1599w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"792\" data-id=\"10936\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result-1024x792.jpg\" alt=\"\" class=\"wp-image-10936\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result-1024x792.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result-600x464.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result-768x594.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result-1110x859.jpg 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/bottom-result.jpg 1313w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure>\n<\/figure>\n\n\n\n<p class=\"has-text-align-center has-text-color has-normal-font-size\" style=\"color:#8b959e\">Temperature results for the top (left) and bottom (right) of the CPU <\/p>\n\n\n\n<h2 class=\"wp-block-heading\">Incorporating the CPU thermal model into a 3D system CFD model<\/h2>\n\n\n\n<p>And here it is. The updated board with the improved CPU underneath the heatsink and fan set up.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"543\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model-1024x543.jpg\" alt=\"CPU thermal model integrated into a PCB thermal analysis 3D system level simulation in Simcenter Flotherm XT.\" class=\"wp-image-10937\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model-1024x543.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model-600x318.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model-768x407.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model-1110x588.jpg 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/clean-model.jpg 1493w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure>\n\n\n\n<p>This is one step closer to creating the complex model\nrequired to determine the best cooling solution for this computer system.<\/p>\n\n\n\n<p>If you would like to know more about Simcenter Flotherm XT, and try it out for yourself, you can with a&nbsp;<a rel=\"noreferrer noopener\" href=\"https:\/\/www.mentor.com\/products\/product-eval\/thermal-design-flotherm-xt-ultra\" target=\"_blank\">free cloud evaluation<\/a>.<\/p>\n\n\n\n<p class=\"has-text-align-center\"><a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/is-my-pc-too-hot\/\">\u2190 Previous<\/a> | <a href=\"https:\/\/blogs.sw.siemens.com\/simcenter\/utilizing-cfd-to-analyse-a-pc-cooling-system\/\">Next \u2192<\/a><\/p>\n","protected":false},"excerpt":{"rendered":"<p>CPU created in Simcenter Flotherm Package Creator The most important component within a typical PC computer is the CPU. So&#8230;<\/p>\n","protected":false},"author":69479,"featured_media":10901,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[242],"industry":[145],"product":[505],"coauthors":[10241],"class_list":["post-10894","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","tag-computational-fluid-dynamics-cfd","industry-electronics-semiconductors","product-simcenter-flotherm-xt"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/6\/2020\/02\/pack.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/10894","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/users\/69479"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/comments?post=10894"}],"version-history":[{"count":4,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/10894\/revisions"}],"predecessor-version":[{"id":48970,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/posts\/10894\/revisions\/48970"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media\/10901"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/media?parent=10894"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/categories?post=10894"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/tags?post=10894"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/industry?post=10894"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/product?post=10894"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/simcenter\/wp-json\/wp\/v2\/coauthors?post=10894"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}