{"id":956,"date":"2022-06-01T09:38:49","date_gmt":"2022-06-01T13:38:49","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/plm-components\/?p=956"},"modified":"2026-03-26T08:03:34","modified_gmt":"2026-03-26T12:03:34","slug":"d-cubed-3d-components-version-59-release","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/plm-components\/d-cubed-3d-components-version-59-release\/","title":{"rendered":"D-Cubed 3D Components version 59 release"},"content":{"rendered":"\n<p>D-Cubed 3D components are integrated by software developers to add 3D modeling capabilities to CAD\/CAM\/CAE and AEC software applications. These applications are used to design, analyze, visualize, and manufacture products from consumer goods to aircraft engines and commercial buildings.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><mark style=\"background-color:rgba(0, 0, 0, 0)\" class=\"has-inline-color has-blue-color\">D-Cubed 3D DCM version 59.0<\/mark><\/h2>\n\n\n\n<p>D-Cubed <a><\/a><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/plm-components\/3d-dcm.html\" target=\"_blank\" rel=\"noopener\">3D DCM<\/a> (3D Dimensional Constraint Manager) is a geometric constraint solving software component. Supporting a wide range of geometries, dimensions and constraints, 3D DCM enables 3D parametric sketching, part shape control using direct modelling, assembly part positioning and kinematic motion simulation. Key enhancements introduced in version 59.0 of D-Cubed 3D DCM are described below.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Model Partitioning<\/h3>\n\n\n\n<p>3D DCM version 59 is now able to automatically divide up unrelated model entities into separate <em>partitions<\/em>. These will be solved independently during a single call to evaluate or similar, which can result in significant performance improvements for larger models that can be partitioned.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Parallel solving<\/h3>\n\n\n\n<p>3D DCM has long supported parallel processing by allowing multiple distinct 3D DCM instances to be created and used in parallel in different threads.<\/p>\n\n\n\n<p>More recent versions of 3D DCM have the capability to use multiple threads within a single 3D DCM instance to perform some <em>relatively limited<\/em> computations in parallel. With version 59 the capability to benefit from multiple threads with a single instance is <em>greatly extended<\/em>. 3D DCM can now perform the majority of the evaluate functions in parallel for each partition in a single 3D DCM instance.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Model accuracy analysis<\/h3>\n\n\n\n<p>When using 3D DCM applications select numerical resolutions to be used in the analysis and solving of dimensions and constraints. These values are defined as a linear resolution and a size value, from which an angular resolution is computed.<\/p>\n\n\n\n<p>Solving is most stable when geometries are either within 1\/10th of the resolutions or separated by 10 times the resolutions. Version 59 of 3D DCM introduces an interface to inform applications when geometry in the model do not conform to these recommendations. This enables adjustments to the resolutions or the modeling approach that better conform to the optimal situation.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><mark style=\"background-color:rgba(0, 0, 0, 0)\" class=\"has-inline-color has-blue-color\">D-Cubed CDM version 59.0<\/mark><\/h2>\n\n\n\n<p>D-Cubed <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/plm-components\/cdm.html\" target=\"_blank\" rel=\"noopener\">CDM<\/a> (Collision Detection Manager) is a software component that offers collision detection and clearance distance measurement for solid, surface, wireframe and point cloud models. It supports accurate, tolerant and faceted geometry. Used in assembly, mechanism, machining and measurement simulation environments, CDM offers a range of algorithms to interactively detect collisions and compute clearances, even on large, complex assemblies. Performance is particularly excellent for common operations, such as repeated computations on models that are in motion. CDM is compatible with most applications, being independent of any modeler or model format. Key enhancements introduced in version 59.0 of D-Cubed CDM are described below.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Enhancements to closest approach functionality<\/h3>\n\n\n\n<p>Version 59 of CDM has functionality that enables the application to enquire all the close approaches between the faces of a pair of bodies within a given capping distance. This builds upon a preliminary version of this capability introduced in version 58.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Performance improvements to closest approach computations<\/h3>\n\n\n\n<p>The performance of closest approach calculations involving large facet nets has been improved in this release.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><mark style=\"background-color:rgba(0, 0, 0, 0)\" class=\"has-inline-color has-blue-color\">D-Cubed HLM version 59.0<\/mark><\/h2>\n\n\n\n<p>D-Cubed&nbsp;<a><\/a><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/plm-components\/hlm.html\" target=\"_blank\" rel=\"noopener\">HLM<\/a>&nbsp;(Hidden Line Manager)) is a software component that provides applications with a fast hidden line computation capability. HLM is optimized for solid, surface and wireframe models, with support for accurate, tolerant and faceted geometry. HLM is compatible with most applications, being independent of modeler or model format. HLM accurately computes hidden line views, engineering drawings and technical illustrations of parts and assemblies with exceptional performance, reliability and functionality. Key enhancements introduced in version 59.0 of D-Cubed HLM are described below.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Improved stability of hidden line computations<\/h3>\n\n\n\n<p>In version 59 of HLM results are more stable for changes to the order in which geometries are added to HLM.<\/p>\n\n\n\n<h2 class=\"wp-block-heading\"><mark style=\"background-color:rgba(0, 0, 0, 0)\" class=\"has-inline-color has-blue-color\">D-Cubed AEM version 59.0<\/mark><\/h2>\n\n\n\n<p>D-Cubed <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/plm-components\/aem.html\" target=\"_blank\" rel=\"noopener\">AEM<\/a> (Assembly Engineering Manager) is a software component that enables applications to simulate the motion of assemblies and mechanisms. It accounts for the mass properties of parts, the motion caused by a range of engineering forces and devices and the interaction of parts as they collide and transmit motion to each other. Key enhancements introduced in version 59.0 of D-Cubed AEM are described below.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Enhancements to contact computations<\/h3>\n\n\n\n<p>AEM has pioneered motion simulations in environments where accurate solid models, not faceted approximations, come into contact and push each other around. This is a more sophisticated process than operating on faceted parts, as there are many more geometry types and configurations involved in computing contact-based motion on full solid parts. The benefits are substantial, including the direct simulation of motion on parts with a geometric accuracy that is suitable for engineering applications, rather than visualization or entertainment. The latest release sees ongoing enhancements to the algorithms used to calculate the contacts when bodies collide.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>D-Cubed 3D components are integrated by software developers to add 3D modeling capabilities to CAD\/CAM\/CAE and AEC software applications. These&#8230;<\/p>\n","protected":false},"author":49853,"featured_media":957,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[91],"tags":[3,34],"industry":[83],"product":[246],"coauthors":[409],"class_list":["post-956","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-product-updates","tag-d-cubed","tag-dcubed-release","industry-software-development","product-plm-open"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/10\/2022\/06\/D-Cubed-3D-components-v59.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/posts\/956","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/users\/49853"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/comments?post=956"}],"version-history":[{"count":2,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/posts\/956\/revisions"}],"predecessor-version":[{"id":959,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/posts\/956\/revisions\/959"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/media\/957"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/media?parent=956"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/categories?post=956"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/tags?post=956"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/industry?post=956"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/product?post=956"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/plm-components\/wp-json\/wp\/v2\/coauthors?post=956"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}