{"id":3610,"date":"2021-06-21T19:09:54","date_gmt":"2021-06-21T23:09:54","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/?p=3610"},"modified":"2026-03-26T09:24:01","modified_gmt":"2026-03-26T13:24:01","slug":"moving-into-metal-cnc-programming-of-the-quadcopters-molds","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/moving-into-metal-cnc-programming-of-the-quadcopters-molds\/","title":{"rendered":"Moving into Metal: CNC Programming of the Quadcopter\u2019s Molds"},"content":{"rendered":"\n<p>In this post, we\u2019ll continue our tour through the Digital Machine Shop as the mold for the plastic top of a quadcopter moves from design into manufacturing.<\/p>\n\n\n\n<p>My name is Lars Okkels, and I am a CAM Consultant here at Siemens Digital Industries Software. As a specialist in the CNC programming of molds, my role was to develop the machining processes that would be used to manufacture the mold for this part. (This mold was designed by Himanshu Iyer using NX Mold Design. He explained his process <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/mold-design-the-quadcopter-launch-begins\/\" target=\"_blank\" rel=\"noreferrer noopener\">here<\/a><\/strong>.)<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-1.png\" alt=\"\" class=\"wp-image-3613\" width=\"490\" height=\"261\"\/><figcaption>Mold for the quadcopter top cover designed in NX CAD Mold Wizard<\/figcaption><\/figure><\/div>\n\n\n\n<p>This was not a highly complex mold, but even so it required 7 mold plates, 1 core insert, 1 cavity insert and 16 electrodes. I\u2019ll focus here on the core and cavity inserts, the mold plates and the ribs on underside of the part. The ribs are the area that necessitated die sink EDM.<\/p>\n\n\n\n<p>In general, my main goal in the CNC programming of molds is to maximize machining efficiency. This guided my work on the quadcopter part\u2019s mold, and I\u2019ll explain below how I used technologies within NX CAM to achieve it. NX is much more than a <strong><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/manufacturing-planning\/cam-software.html\" target=\"_blank\" rel=\"noreferrer noopener\">CAM software<\/a><\/strong>&nbsp;&#8211; it\u2019s a complete part manufacturing solution, with advanced functionality such as simulation and process wizards that allowed me to work efficiently and to optimize the manufacturing processes involved here.<\/p>\n\n\n\n<p>In addition to machine efficiency, my other critical goal, as a moldmaker, for this project is producing a very smooth surface on the cavity. It would form the top of the plastic part \u2013 the visible area that would give people their overall impression of the quadcopter. Also, I wanted to avoid mistakes in production that would slow the project, such as finding out that tools were too short, for instance, or that clamping needed to be moved. NX CAM helped me address these considerations as well.<\/p>\n\n\n\n<div class=\"wp-block-cover alignfull is-light\"><span aria-hidden=\"true\" class=\"has-background-dim-100 wp-block-cover__gradient-background has-background-dim has-background-gradient\" style=\"background:linear-gradient(135deg,rgb(238,238,238) 31%,rgb(169,184,195) 100%)\"><\/span><div class=\"wp-block-cover__inner-container is-layout-flow wp-block-cover-is-layout-flow\">\n<div class=\"wp-block-media-text alignwide is-stacked-on-mobile is-vertically-aligned-center is-image-fill\" style=\"grid-template-columns:52% auto\"><figure class=\"wp-block-media-text__media\" style=\"background-image:url(https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-961x1024.jpg);background-position:50% 50%\"><img loading=\"lazy\" decoding=\"async\" width=\"961\" height=\"1024\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-961x1024.jpg\" alt=\"NX CAM software and CNC programming of molds helps machine shops automate part manufatcuring.\" class=\"wp-image-4221 size-full\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-961x1024.jpg 961w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-563x600.jpg 563w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-768x818.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-1442x1536.jpg 1442w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-1922x2048.jpg 1922w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/CAM_software-900x959.jpg 900w\" sizes=\"auto, (max-width: 961px) 100vw, 961px\" \/><\/figure><div class=\"wp-block-media-text__content\">\n<h2 class=\"has-text-color wp-block-heading\" style=\"color:#000000;font-size:32px\">Automate Your Machine Shop to Gain an Advantage, Today<\/h2>\n\n\n\n<p class=\"has-text-color\" style=\"color:#000000;font-size:17px\">Watch this webinar to learn how Siemens NX software for CAD, CAM, CMM, robotics, and additive manufacturing can help you stay competitive through automation in part manufacturing.<\/p>\n\n\n\n<div class=\"wp-block-buttons is-layout-flex wp-block-buttons-is-layout-flex\">\n<div class=\"wp-block-button is-style-fill\"><a class=\"wp-block-button__link\" href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/webinar\/machine-shop-automation\/63958\" target=\"_blank\" rel=\"noreferrer noopener\"><strong><mark style=\"background-color:rgba(0, 0, 0, 0)\" class=\"has-inline-color has-white-color\">Watch now<\/mark><\/strong><\/a><\/div>\n<\/div>\n<\/div><\/div>\n<\/div><\/div>\n\n\n\n<h2 class=\"wp-block-heading\">The digital thread continues<\/h2>\n\n\n\n<p>Similar to the way that mold design began with CAD data, the starting point for me was also digital, i.e. Himanshu\u2019s NX file of the mold design. It was nice knowing that he had used the Digital Twin approach and the technologies available to him in <strong><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/manufacturing-planning\/tooling-fixture-design.html\" target=\"_blank\" rel=\"noreferrer noopener\">NX Mold Design<\/a><\/strong>&nbsp;to ensure that the part was actually moldable. He also made sure that the mold was optimized for performance, for example by use of features such as conformal cooling channels to shorten the cooling time.<\/p>\n\n\n\n<p>I also used the Digital Twin approach, which for <strong><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/manufacturing-planning\/cnc-programming.html\" target=\"_blank\" rel=\"noreferrer noopener\">CNC programming<\/a><\/strong>&nbsp;of molds means working in the context of the complete machine setup and having connectivity to the original model design. This helps me program any job faster and simulate operations to optimize them prior to sending them to the shop floor. The cavity insert offers a good example of this.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Cavity programming &nbsp;<\/h3>\n\n\n\n<p>With inserts, you\u2019re typically making only one or two parts, so it\u2019s important to get them right the first time. Machining, particularly roughing, of hard materials used for molds can take a long time if you use conventional machining methods. To speed up the process, I used NX\u2019s Adaptive Milling, a high-speed machining (HSM) method that enables deep cuts at high cutting rates. It can shorten roughing cycle of the toughest materials by 60%.<\/p>\n\n\n\n<p>As I mentioned earlier, a key goal in milling the cavity was to achieve a super smooth surface. This was obvious to me since the top of the quadcopter is a visible part. But also, the mold designer conveyed the desired surface quality and tolerances by using product and manufacturing information (PMI) added to the 3D model of this mold.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2-1024x576.png\" alt=\"\" class=\"wp-image-3614\" width=\"768\" height=\"432\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2-1024x576.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2-600x337.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2-768x432.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2-900x506.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-2.png 1521w\" sizes=\"auto, (max-width: 768px) 100vw, 768px\" \/><figcaption><em>NX CAM Adaptive Milling\u2019s smooth cutting patterns enable deep cuts at high machining speeds while managing the tool load,<\/em> <em>which accelerates machining and extends tool life.<\/em><\/figcaption><\/figure><\/div>\n\n\n\n<p>Surface quality involves the interplay of many variables including cutting strategies, speeds, feeds, the choice of cutting tools, etc. I used my previous experience in the CNC programming of molds and the advanced toolpath technologies in NX in the process. For instance, to follow the natural shapes of the mold shape, I used the Guiding Curves finishing that generates smooth-flowing toolpath that result in excellent surface finish.<\/p>\n\n\n\n<p>The G code-driven simulation functionality within NX CAM is great way to validate the machining process. On my screen, I could observe material removal, machine moves and so on, and quickly make changes to optimize surface quality.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Core programming<\/h3>\n\n\n\n<p>The strengthening ribs added by the designer to the underside of the part affected how I programmed the milling of the core. The sharp angles created by the ribs necessitated the use of die sink EDM. But before using EDM, I needed to rough that area as quickly as possible without machining the rib details. NX CAM has a great feature called Geometry Wave Linker that allowed me to make changes to geometry of the core insert without affecting the CAD model, while maintaining associativity to the original design. I simplified the geometry of the rib area to optimize the toolpath, which helps me shorten machining time.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"189\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3-1024x189.png\" alt=\"\" class=\"wp-image-3615\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3-1024x189.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3-600x111.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3-768x142.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3-900x166.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-3.png 1320w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption><em>NX\u2019s Synchronous Technology enables engineers to directly edit the part model and prepare it for NC programming, including closing holes and gaps, offsetting faces and resizing part features<\/em>.<\/figcaption><\/figure><\/div>\n\n\n\n<p>Electrodes are used for the die sink EDM process. This core needed 16 electrodes, but some molds require hundreds, so the ability to automate electrode programming is essential. Siemens provides this through the NX Electrode Design Wizard. It guided me through a step-by-step workflow to design the electrodes. It lets you specify things like extension height, draft angle, material and spark gaps. That, in combination with various Synchronous Modeling functions, allowed me to define the electrode geometry (offsetting faces or adding blends) to allow for a better EDM process.<\/p>\n\n\n\n<div class=\"wp-block-columns is-layout-flex wp-container-core-columns-is-layout-9d6595d7 wp-block-columns-is-layout-flex\">\n<div class=\"wp-block-column is-layout-flow wp-block-column-is-layout-flow\">\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"620\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1-1024x620.png\" alt=\"\" class=\"wp-image-3616\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1-1024x620.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1-600x363.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1-768x465.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1-900x545.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.1.png 1450w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><\/div>\n<\/div>\n\n\n\n<div class=\"wp-block-column is-layout-flow wp-block-column-is-layout-flow\">\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"620\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2-1024x620.png\" alt=\"\" class=\"wp-image-3617\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2-1024x620.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2-600x363.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2-768x465.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2-900x545.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-4.2.png 1450w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><\/figure><\/div>\n<\/div>\n<\/div>\n\n\n\n<p class=\"has-text-align-center\"><em>The smooth-flowing Guiding Curves operation in NX CAM is an ideal cutting method for high-speed finishing<\/em><\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Mold plate programming<\/h3>\n\n\n\n<p>Mold plates are the parts in the mold assembly that hold the core and cavity inserts in place. A mold typically has seven or eight plates, which are characterized by many pockets, holes, slots, etc. Although these features are not complex, programming them can take a lot of time and manual selections. NX CAM provides the capability to automate the programming of mold plates. Using this automation functionality, some of our customers have reduced programming time for mold plates by more than 90 percent.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-5.jpg\" alt=\"\" class=\"wp-image-3618\" width=\"659\" height=\"399\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-5.jpg 879w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-5-600x363.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-5-768x465.jpg 768w\" sizes=\"auto, (max-width: 659px) 100vw, 659px\" \/><figcaption><em>With Feature-based machining (FBM) in NX CAM, you can automatically create optimized machine programs directly from part design models. FBM automatically recognizes and programs a wide range of machining feature types, such as pockets, holes and slots.<\/em><\/figcaption><\/figure><\/div>\n\n\n\n<p>The automation helps you speed up the programming of the plates so you can dedicate your time to the more complicated parts like the core and cavity inserts. For the quadcopter mold, I took advantage of two capabilities of NX CAM to accelerate the task: feature-based machining (FBM) and the ability to use the PMI information from the original CAD model to further automate the process.<\/p>\n\n\n\n<p>Feature-based machining in NX CAM is very powerful. In this case, it started by analyzing the plate geometry and identifying features such as holes (simple or compound), pockets, notches, slots, etc. The basic functionality out-of-the-box can recognize more than 70 features, but you can also define your own. Because these plates are often machined from multiple sides, you can choose to recognize features from specific directions or from all directions. I opted to have it recognize features from both top and bottom machining directions.<\/p>\n\n\n\n<p>Once the features were identified, NX CAM automatically programmed the toolpaths, using tolerance data included in the PMI to ensure that required tolerances would be held. It\u2019s very fast. For example, it took me less than five minutes to program the ejector plate, which can take hours to program using conventional methods. In addition to greatly reducing programming time, another benefit of feature-based machining is that it ensures a consistent machining process by all levels of programmers.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-6.jpg\" alt=\"\" class=\"wp-image-3619\" width=\"660\" height=\"372\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-6.jpg 880w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-6-600x338.jpg 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-6-768x433.jpg 768w\" sizes=\"auto, (max-width: 660px) 100vw, 660px\" \/><figcaption><em>Programmers can create complete machining process for mold plates, like the one shown here, in a matter of minutes using FBM in NX CAM. It not only automates programming, it also standardizes processes, ensuring use of the company best practices.<\/em><\/figcaption><\/figure><\/div>\n\n\n\n<h3 class=\"wp-block-heading\">Machining process validation<\/h3>\n\n\n\n<p>Since much of my work is aimed at maximizing machining efficiency, and one aspect of that involves reducing down time, I appreciate the G-code driven simulation functionality in NX CAM.<\/p>\n\n\n\n<p>The <strong><a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/products\/manufacturing-planning\/postprocessing-machining-simulation.html\" target=\"_blank\" rel=\"noreferrer noopener\">simulation capability<\/a><\/strong> is a perfect example of how a Digital Twin replicates the real world. Siemens has relationships with all of the major machine tool manufacturers and they have worked with us to build exact virtual replicas of their machines. These replicas are incorporated into the simulation functionality of NX CAM. Working with a precise digital copy of the milling machine gave me confidence that I was getting smooth, efficient tool motions and consistent tool path quality, and that the CNC programs I would be sending to the shop floor were error-free. For example, using the integrated simulation I was able to ensure that we didn\u2019t find other problems on the shop floor, such as tools that were too short, or clamping that wasn\u2019t right.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"582\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-1024x582.png\" alt=\"\" class=\"wp-image-3635\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-1024x582.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-600x341.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-768x437.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-1536x873.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1-900x512.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1.png 1574w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption><em>A key NX CAM advantage facilitates integrated simulation and verification of the NC programs (or G-code), which enables programmers<\/em> <em>to check tool paths within the NC programming session.<\/em><\/figcaption><\/figure><\/div>\n\n\n\n<p>Without this type of simulation, a machine operator could have performed a dry run on the actual machine, but this would have taken that machine out of operation, which can negatively impact your productivity.<\/p>\n\n\n\n<h3 class=\"wp-block-heading\">Postprocessing &amp; shop floor docs<\/h3>\n\n\n\n<p>Postprocessing involves generating the NC program (or G code) to drive the CNC machines on the shop floor. It is one of the critical steps as you transition from planning to production, since you need to \u201ctranslate\u201d the toolpaths that your created into a code for your specific controller-machine configuration. As a user of NX CAM, I have access to more than 1,000 postprocessors stored in the cloud-based <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/post-hub-a-cloud-based-postprocessor-solution-for-nx-cam-software\/\" target=\"_blank\" rel=\"noreferrer noopener\">Post Hub<\/a><\/strong>. I didn\u2019t need to leave NX to access the online library, and it was very easy to use. I simply selected my machine and controller and Post Hub showed me the applicable postprocessors. I generated the desired NC program using the postprocessor that I selected. But if I needed to make a modification in the output, I could have used Post Configurator, which is very simple to use.<\/p>\n\n\n\n<p>In addition to G code, I generated complete documentation for the shop floor, including tooling data and work instructions. All of this output was also generated automatically with NX CAM.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-8.png\" alt=\"\" class=\"wp-image-3621\" width=\"506\" height=\"389\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-8.png 1012w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-8-600x461.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-8-768x590.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-8-900x691.png 900w\" sizes=\"auto, (max-width: 506px) 100vw, 506px\" \/><figcaption><em>NX CAM helps you generate a complete shop documentation, including setup sheets and tool lists, digitally connecting CNC programmers with the machine operators. It ensures a quick setup and error-free production.<\/em><\/figcaption><\/figure><\/div>\n\n\n\n<p><br>The advanced machining methods discussed in this blog helps moldmakers shorten machining time and improve surface finish quality. At the same time, the latest toolpath technologies help manufacturers extend tool life and improve machine performance, reducing production costs. The digitally validated toolpaths eliminate the need for physical test cuts that can increase machine uptime and virtually eliminate scrap.<\/p>\n\n\n\n<div class=\"wp-block-cover alignfull is-light\"><span aria-hidden=\"true\" class=\"has-background-dim-100 wp-block-cover__gradient-background has-background-dim has-background-gradient\" style=\"background:linear-gradient(135deg,rgb(238,238,238) 31%,rgb(169,184,195) 100%)\"><\/span><div class=\"wp-block-cover__inner-container is-layout-flow wp-block-cover-is-layout-flow\">\n<div class=\"wp-block-media-text alignwide is-stacked-on-mobile is-vertically-aligned-center is-image-fill\" style=\"grid-template-columns:52% auto\"><figure class=\"wp-block-media-text__media\" style=\"background-image:url(https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/JK-Machining-machine-shop.png);background-position:50% 50%\"><img loading=\"lazy\" decoding=\"async\" width=\"770\" height=\"442\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/JK-Machining-machine-shop.png\" alt=\"Automation and CNC programming of molds helps JK Machining thrive in a competitive marketplace\" class=\"wp-image-4222 size-full\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/JK-Machining-machine-shop.png 770w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/JK-Machining-machine-shop-600x344.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/JK-Machining-machine-shop-768x441.png 768w\" sizes=\"auto, (max-width: 770px) 100vw, 770px\" \/><\/figure><div class=\"wp-block-media-text__content\">\n<h2 class=\"has-text-color wp-block-heading\" style=\"color:#000000;font-size:32px\">Automation helps a machine shop thrive in a competitive marketplace<\/h2>\n\n\n\n<p class=\"has-text-color\" style=\"color:#000000;font-size:17px\">Learn how NX enables JK Machining to increase efficiency with a digital thread throughout the entire mold design and manufacturing process.<\/p>\n\n\n\n<div class=\"wp-block-buttons is-layout-flex wp-block-buttons-is-layout-flex\">\n<div class=\"wp-block-button is-style-fill\"><a class=\"wp-block-button__link\" href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/our-story\/customers\/jk-machining\/49216\/\" target=\"_blank\" rel=\"noreferrer noopener\"><strong><span class=\"has-inline-color has-white-color\">Learn more<\/span><\/strong><\/a><\/div>\n<\/div>\n<\/div><\/div>\n<\/div><\/div>\n\n\n\n<p>The next post will cover another important step in the quadcopter part\u2019s development \u2013 additive manufacturing, which was used to create the conformational cooling channels on the mold.<\/p>\n\n\n\n<p>If you\u2019d like to learn more about my world, check out <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/one-software-solution-for-the-mold-manufacturing-process\/\" target=\"_blank\" rel=\"noreferrer noopener\">my blog post about mold manufacturing<\/a><\/strong>.<\/p>\n\n\n\n<p>Read the first blog in our digital machine shop series <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/the-digital-machine-shop-making-an-idea-go-airborne\/\" target=\"_blank\" rel=\"noreferrer noopener\">here<\/a><\/strong>, catch up on the previous blog on mold design <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/mold-design-the-quadcopter-launch-begins\/\" target=\"_blank\" rel=\"noreferrer noopener\">here<\/a><\/strong>, and read the next blog in the series on additive manufacturing <strong><a href=\"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/getting-closer-to-launch-additive-manufacturing-for-the-quadcopter-mold\/\" target=\"_blank\" rel=\"noreferrer noopener\">here<\/a><\/strong>.<\/p>\n\n\n\n<div class=\"wp-block-image\"><figure class=\"aligncenter size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-1024x572.png\" alt=\"\" class=\"wp-image-3622\" width=\"768\" height=\"429\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-1024x572.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-600x335.png 600w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-768x429.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-1536x858.png 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9-900x503.png 900w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-9.png 1598w\" sizes=\"auto, (max-width: 768px) 100vw, 768px\" \/><figcaption><em>The advanced toolpath technologies in NX CAM enable shorter machining time and better surface finish, accelerating the manufacturing of high-quality molds.<\/em><\/figcaption><\/figure><\/div>\n","protected":false},"excerpt":{"rendered":"<p>In this post, we\u2019ll continue our tour through the Digital Machine Shop as the mold for the plastic top of&#8230;<\/p>\n","protected":false},"author":61637,"featured_media":3635,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[161],"tags":[168,218,201],"industry":[129,139,141],"product":[309,487],"coauthors":[840],"class_list":["post-3610","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-learning-resources","tag-computer-aided-design-cad","tag-digital-machine-shop","tag-mold-design","industry-consumer-industrial-electronics","industry-industrial-machinery","industry-mold-tool-die","product-nx","product-nx-cam"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2021\/06\/Image-7.1.png","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/3610","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/users\/61637"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/comments?post=3610"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/3610\/revisions"}],"predecessor-version":[{"id":4226,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/3610\/revisions\/4226"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/media\/3635"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/media?parent=3610"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/categories?post=3610"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/tags?post=3610"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/industry?post=3610"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/product?post=3610"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/coauthors?post=3610"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}