{"id":2108,"date":"2013-05-30T06:00:00","date_gmt":"2013-05-30T13:00:00","guid":{"rendered":"https:\/\/blogs.plm.automation.siemens.com\/t5\/News-NX-Manufacturing\/In-Simulation-We-Trust\/ba-p\/1706"},"modified":"2026-03-26T09:19:06","modified_gmt":"2026-03-26T13:19:06","slug":"in-simulation-we-trust","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/in-simulation-we-trust\/","title":{"rendered":"In Simulation We Trust"},"content":{"rendered":"<p><P><EM>This article appeared in MoldMaking Technology magazine, Gardner Publications, Inc., USA. <a href=\"http:\/\/www.moldmakingtechnology.com\" target=\"_blank\" rel=\"nofollow noopener noreferrer\">www.moldmakingtechnology.com<\/A><\/EM><\/P><\/p>\n<p><P><IMG src=\"https:\/\/siemensplm.i.lithium.com\/t5\/image\/serverpage\/image-id\/526iE78D87F7C2A71606\/image-size\/large?v=mpbl-1&amp;px=-1\" border=\"0\" alt=\"NX 8.5 Mold Flow Simulation\" title=\"NX 8.5 Mold Flow Simulation\" align=\"center\" \/><\/P><br \/>\n<P><EM>Some CAD systems come equipped with directly integrated mold flow simulation capabilities that help save time setting up simulations, checking designs, and evaluating design alternatives. <a href=\"https:\/\/blogs.plm.automation.siemens.com\/t5\/TV\/Analyze-Mold-Flow-in-NX\/ba-p\/1715\" target=\"_blank\" rel=\"noopener noreferrer\">Watch a video on Mold Flow Analysis inside NX.<\/A><\/EM><\/P><\/p>\n<p><P>We all know that simulation technology delivers benefits but, as with most technology, we don\u2019t typically take full advantage of it. Simulation has a lot to offer to mold manufacturing. It\u2019s a matter of recognizing the problems that it can help solve.<\/P><\/p>\n<p><P>While we challenge ourselves to find new ways to compete, take on tougher jobs, diversify into new markets and even add new product lines, today\u2019s economic climate dictates that not only must we deliver a job done well, but we must get it done right the first time around. For this reason, the need for simulation technology has become inescapable for mold manufacturers.<\/P><\/p>\n<p><P>Simulation technology has the ability to help optimize parts designs, predict mold performance and validate our decisions. With simulation-driven best practices we can tackle the most complicated jobs\u2014and do them while facing the pressures of overly-aggressive schedules and scarce resources. It can also help achieve business objectives by avoiding costly mistakes that result in inaccurate quotes, incorrectly estimated cycle times, errors in production, wasted material, as well as process inefficiencies.<\/P><\/p>\n<p><P>The following is a brief look at some recent trends in simulation technology as they pertain to key areas of plastic part production and how to take advantage of it from design through manufacturing.<\/P><\/p>\n<p><P><FONT size=\"2\"><STRONG><FONT color=\"#000000\">Design Better Parts Faster<\/FONT><\/STRONG><\/FONT><\/P><br \/>\n<P>Continued advances in simulation technology have made it possible to turn more ideas into volume production much less expensively than before. Part designers can use simulation to understand the relationships between part design, mold design, material and molding conditions which affect appearance, material selection, molding machine requirements, as well as cycle time.<\/P><\/p>\n<p><P>Ease-of-use improvements to Finite Element Analysis (FEA) tools\u2014such as integration directly into the CAD environment and automatic generation of 3D mesh models\u2014enable designers to easily set up and run simulations to predict the strength, vibration, flow and fill performance of designs. While advanced capabilities for simulating specialized molding processes like insert molding, over-molding and multi-shot sequential molding give designers the freedom to explore more complex, innovative designs without the need for physical prototypes.<\/P><\/p>\n<p><P>In automotive for example, fuel prices and the continuing climate debate have stimulated an increase in lightweight materials usage to reduce the overall weight of vehicles and thus contribute to lower fuel consumption and emissions, while maintaining safety. With advances in the modeling of the anisotropy of reinforced plastics and improvements, crash and fatigue life prediction simulations are promoting the discovery and prove-out of innovative alternatives to standard designs. As a result it seems that just about every vehicle component could be up for a makeover\u2014lightweight replacements for brake pedals, door systems, shock absorbers, and even axle systems are on their way to volume production now.<\/P><\/p>\n<p><P>While a part can be manufactured to specification and dimensionally correct, if it has a visual defect, it\u2019s scrapped. For parts that depend on appearance, designers are using filling simulation to predict melt front progression and to guide their decision-making and avoid design elements that, when manufactured, can render parts visually unacceptable. Mold flow issues such as weld lines, air traps, short shots and sink marks can all be properly accounted for during the design phase. In some cases, these mold filling issues can affect physical performance as well, as in the case of weld lines in fiber-reinforced materials.<\/P><\/p>\n<p><P><FONT size=\"2\"><STRONG><FONT color=\"#000000\">Make More Complex, Higher Quality and Better Performing Molds<\/FONT><\/STRONG><\/FONT><\/P><br \/>\n<P>Foreign competition is evaporating the margin on simple tools, driving the need to take on more complex jobs. What&#8217;s more, the complexity of parts is rapidly surpassing the in-house know-how needed to mold them. Fortunately, simulation-driven design methods can address a range of issues in order to help engineer more complex, higher quality and better performing molds.<\/P><\/p>\n<p><P>Because of simulation, the trial-and-error approach to prove-out tools on the shop floor is rapidly becoming a practice of the past.<\/P><\/p>\n<p><P>Beyond just the simple interference and clearance analyses, tool kinematic motion and assembly \/ disassembly can now be digitally simulated and validated directly inside the CAD system. Runner systems and gate configurations can be evaluated and molding and pressure drop issues avoided without conducting any actual tool try-outs by using mold filling and cooling simulation to determine optimum gate positions and balance melt flow.<\/P><\/p>\n<p><P>Slow cycle times decrease a company\u2019s cost advantage. Inadequate thermal management within a mold is a common contributor to poor tool performance. Cooling time can occupy the majority of an injection cycle and can also contribute to non-uniform shrinkage\u2014leading to warpage issues. By simulating true 3D material flow through the mold cavity and the heat transfer from the injected plastic to the water lines, it\u2019s possible to optimize a mold\u2019s design to achieve optimum fill and cooling times. Cooling analysis can also be used to determine ejection temperature &#8211; the earliest acceptable time to eject &#8211; and the optimum locations for and number of ejector pins.<\/P><\/p>\n<p><P>Furthermore, simulation can directly affect profitability by improving the accuracy of quoting and costing activities. By using mold flow simulation technology it is possible to avoid overestimating cycle times, which often results in not winning new business and underestimating that can reduce profits. FEA-based strength analysis and simulation can also be used to assess if a tool is overbuilt and how much excess material (and cost) can be safely eliminated.<\/P><\/p>\n<p><P><FONT size=\"2\"><STRONG><FONT color=\"#000000\">Create Error-Free Programs Faster and Machine More Efficiently<\/FONT><\/STRONG><\/FONT><\/P><br \/>\n<P>Machining simulation is prevalently used by NC programmers to get error-free and optimized programs to the shop floor faster. \u201cProving out\u201d NC programs digitally prior to machining can save significant job costs. Scrapped parts, material wastage, broken tools and machine crashes are examples of the costly issues that can be avoided. Machining simulation capabilities have even matured to where they can be relied upon to run a first-time part unattended. As a result, many companies have made simulation a standard process step, requiring all programs be verified prior to releasing to the shop floor.<\/P><br \/>\n<P><FONT face=\"Times New Roman\" size=\"3\" color=\"#000000\">&nbsp;<\/FONT><\/P><br \/>\n<P><FONT face=\"Times New Roman\" size=\"3\" color=\"#000000\"><IMG src=\"https:\/\/siemensplm.i.lithium.com\/t5\/image\/serverpage\/image-id\/527i543DBC37016DE973\/image-size\/large?v=mpbl-1&amp;px=-1\" border=\"0\" alt=\"Virtual Machine Tool in NX\" title=\"Virtual Machine Tool in NX\" align=\"center\" \/><\/FONT><\/P><br \/>\n<P><EM>A Virtual Machine Tool inside the CAM system can be used for postprocessed NC code validation, setup, training, and even manual editing of NC code just like at the real, physical machine. <a href=\"https:\/\/blogs.plm.automation.siemens.com\/t5\/TV\/Virtual-Machine-inside-NX-CAM\/ba-p\/1713\" target=\"_blank\" rel=\"noopener noreferrer\">Watch a video the Virtual Machine Tool inside NX CAM.<\/A><\/EM><\/P><\/p>\n<p><P>As more 5-axis and multi-function machines are commissioned for mold machining, simulation will play a more prominent role in the NC programming process. While these complex machine tools can reduce the number of setups, machine faster and produce a better surface finish, they also are considerably more complicated to program and there is greater potential for crashes and gouges, thus driving the need to verify programs in the context of the machine tool using machine tool simulation.<\/P><\/p>\n<p><P>Machine tool simulation comes in various levels of capability that can serve different purposes:<\/P><\/p>\n<p><P><STRONG><EM>Toolpath-driven machine tool simulation <\/EM><\/STRONG>drives a 3D machine model simulation straight from the internal toolpath records of the CAM system. It is the quickest at producing a result, but may not be the most accurate because it doesn\u2019t use or verify the actual postprocessed output.<\/P><\/p>\n<p><P><STRONG><EM>G-code driven machine tool simulation<\/EM><\/STRONG> provides a complete kinematic 3D machine environment for visualizing complex motion. Collision checking and multi-channel synchronization is simulated with the postprocessed g-code output so home positions, special tool change motion, and other content inserted by the postprocessor are checked, minimizing any surprises at the machine tool.<\/P><br \/>\n<P><FONT color=\"#000000\">&nbsp;<\/FONT><\/P><br \/>\n<P><STRONG><EM>G-code driven simulation with embedded virtual NC controller kernel (VNCK)<\/EM><\/STRONG> uses the actual controller software to process the posted output exactly as it would on the real machine and drives the kinematic 3D machine tool model to display the simulation. Instead of relying on generic software approximation, this integrated approach computes accurate machining times for each operation and for the entire machining sequence by considering a complete model of the machine that accounts for its performance and response. This approach provides the greatest level of accuracy and completeness.<\/P><\/p>\n<p><P><EM><STRONG>A virtual machine tool<\/STRONG> <\/EM>is a virtual copy of a physical machine tool with exactly the same controller, features, HMI and operator panel. It can be used for training, setup, postprocessed NC code validation and even manual editing of NC code just like at the real, physical machine. Machine tool builders that offer the virtual machines can use it to reproduce issues found at customer sites.<\/P><\/p>\n<p><P>Lastly, some CAM systems are making it easier to create optimized and error-free programs by <EM>integrating the complete array of machine tool simulation capabilities right into the NC programming environment<\/EM>. The simulation information is right at hand where it\u2019s needed to make any adjustments or corrections. This approach also eliminates extra steps required for data translation and transfer, design iterations and engineering changes, as well as additional software administration.<\/P><\/p>\n<p><P><IMG src=\"https:\/\/siemensplm.i.lithium.com\/t5\/image\/serverpage\/image-id\/528i254A7C5C22D6DA23\/image-size\/large?v=mpbl-1&amp;px=-1\" border=\"0\" alt=\"Virtual NC Controller Kernel\" title=\"Virtual NC Controller Kernel\" align=\"center\" \/><\/P><br \/>\n<P><EM>G-code driven VNCK simulation can reveal issues resulting from unwanted repositioning of the rotary machine tool axes near a kinematic singularity of the machine tool. This can be simply fixed by adjusting the tool tilt angle in the CAM system.<\/EM><\/P><\/p>\n<p><P>In addition, CAM systems are now using aspects of simulation technology to provide a more comprehensive and <EM>interactive programming experience<\/EM>\u2014like creating toolpaths by dragging and tilting the cutting tool (along with the machine) in the scene or displaying the current material condition of the part as it progresses through each step of the process.<\/P><\/p>\n<p><P><FONT size=\"2\"><STRONG><FONT color=\"#000000\">Summary<\/FONT><\/STRONG><\/FONT><\/P><br \/>\n<P>Simulation technology can make a significant impact on all phases of plastic part production, from design through manufacturing. In addition to helping avoid costly errors by checking work before doing it for real, this technology can assist in making better decisions that result in better parts, better performing tools and more efficient manufacturing processes. Simulation technology is available inside some CAD\/CAM systems and through stand-alone applications. Either way, significant time and material benefits can be gained by using it.<\/P><\/p>\n<p><P><STRONG><FONT size=\"2\">About the Author<\/FONT><\/STRONG><\/P><br \/>\n<TABLE border=\"1\" cellpadding=\"1\" align=\"left\"><br \/>\n<TBODY><br \/>\n<TR><br \/>\n<TD width=\"80\"><IMG src=\"https:\/\/siemensplm.i.lithium.com\/t5\/image\/serverpage\/image-id\/33i8DBBF25B900A9DA8\/image-size\/original?v=mpbl-1&amp;px=-1\" border=\"0\" alt=\"Community.jpg\" title=\"Community.jpg\" width=\"80\" align=\"center\" \/><\/TD><br \/>\n<TD>Aaron Frankel is with the marketing team at Siemens PLM Software and focuses on part manufacturing solutions. He has been in the PLM industry for over 15 years and enjoys helping companies apply innovative technology solutions to design and manufacturing challenges. Aaron resides in Southern California with his family.<\/TD><br \/>\n<\/TR><br \/>\n<\/TBODY><br \/>\n<\/TABLE><\/p>\n","protected":false},"excerpt":{"rendered":"<p>This article appeared in MoldMaking Technology magazine, Gardner Publications, Inc., USA. www.moldmakingtechnology.com <\/p>\n<p> Some CAD systems come equipped with directly integrated mold flo&#8230;<\/p>\n","protected":false},"author":61920,"featured_media":2112,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[169],"industry":[],"product":[],"coauthors":[],"class_list":["post-2108","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-news","tag-computer-aided-manufacturing-cam"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/15\/2019\/09\/Community-6.jpg","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/2108","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/users\/61920"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/comments?post=2108"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/2108\/revisions"}],"predecessor-version":[{"id":2114,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/posts\/2108\/revisions\/2114"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/media\/2112"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/media?parent=2108"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/categories?post=2108"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/tags?post=2108"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/industry?post=2108"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/product?post=2108"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/nx-manufacturing\/wp-json\/wp\/v2\/coauthors?post=2108"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}