Atos and MindSphere: Faster toward digitalization

Atos and MindSphere: Faster toward digitalization

2018-04-23 07.22.15_P4-EM2_2884.jpg

Accelerate the digital journey! Atos and MindSphere will once again joined forces to present their solutions for the cloud-based, open IoT operating system in the MindSphere Lounge at Hannover Messe 2018. This just in: MindSphere on premise – for customers with the highest data protection standards.

Atos, a strategic partner of Siemens, has developed an agile end-to-end approach to MindSphere-based IoT services that creates measurable benefits quickly and reliably. The Atos apps for MindSphere are tightly integrated with the Atos Codex Services for MindSphere. The apps provide a reliable data source that can be used for efficient analyses and cognitive computing and as a platform on which customers can develop agile business processes.

Use cases and apps for many industries

At Hannover Messe, Atos provided insights into its services, from consulting, designing application scenarios, prototyping, and application development to integration and commissioning. The company is using industry-specific use cases and applications to showcase how car manufacturers, chemical, utility, and transport companies, the food and beverage industry, machine builders, and even financial service providers can benefit from these services.

The range of Atos MindSphere apps is constantly growing, and examples include Maintenance Planner, Container Management, and Manufacturing Sustainability. With the latter app, plant operators and quality managers can measure energy consumption and emissions and compare them with pre-defined targets. This makes it possible to create detailed sustainability profiles, detect irregularities in real time, and minimize energy consumption.


                                                                                                                     


Consultancy services from Atos – which trade fair visitors learned about in the MindSphere Lounge – are based on these use cases and on applications developed in-house for MindSphere. Experts in the MindSphere Lounge explained how Atos helps companies accelerate their time to value on their path toward digitalization. At the heart of the solution, MindSphere also allows customers to develop their own agile apps to improve the efficiency, performance, and output of their production.

Even greater security for data: MindSphere on premise


Atos is currently working with Siemens on a solution to operate MindSphere in a highly secure private cloud environment: MindSphere on premise responds to the needs of customers that have extremely high requirements for a secure data environment, latency time, or compliance with legal regulations. These customers can use the solution to deploy and manage their own MindSphere applications locally. MindSphere on premise will be available at the end of 2018.

Leave a Reply