JT2Go mobile adds a cross section feature

Dynamic Cross Sectioning is now available in JT2Go on iOS and Android. Users are able to create cross sections of their displayed models that can be dynamically positioned in the defined plane. Once a section is created, using either the “X”, “Y” or  “Z” planes, the plane can be dragged on the plane vector using finger gestures. Multiple planes can be enabled in the same view. Clipping can be applied to either the near or far side of the defined plane. Users can remove the last plane added or all planes defined in the view.



Cross section feature.PNG

Leave a Reply