Digital crude oil models: Design exploration at scale for oil and gas innovation
In oil and gas, the challenge is no longer only to understand crude oil: it is to explore, compare, and redesign chemical systems faster than experimentation allows. Whether the goal is flow assurance, formulation screening, chemical production or materials optimization, innovation today depends on how efficiently complex crude systems can be represented, modified and explored in silico.
This is where digital crude oil models come into play. Not as static representations, but as living, design-ready models that engineers can manipulate, adapt and connect to automated exploration workflows. With Simcenter Culgi, digital crude oil modeling becomes a practical, scalable foundation for chemical design exploration across the oil and gas value chain.
From crude oil complexity to actionable digital models
Crude oil is one of the most complex industrial fluids: thousands of components, broad distributions of molecular sizes and functionalities, and strong sensitivity to temperature, pressure and composition. Modeling such systems at full atomistic resolution is neither necessary nor efficient for most engineering questions.
Modern digital crude oil models take a fit-for-purpose approach:
- Preserve the chemical diversity that drives macroscopic behavior
- Reduce unnecessary molecular detail
- Focus on properties that matter for engineering decisions
In Simcenter Culgi, crude oils are represented using experimentally grounded digital models, typically built from:
- SARA fractions (saturates, aromatics, resins, asphaltenes)
- Density and compositional ranges
- Acid number (TAN) and polar content
- Additional field‑relevant descriptors when needed
The result is a digital crude oil that behaves like the real one, but is computationally tractable and, crucially, easy to modify, recombine and explore with our Mixture editor capability:
This is not about recreating every molecule. It is about enabling design exploration on systems that remain chemically relevant.
Full crude or targeted chemistry: One framework, multiple scales
A key strength of this approach is flexibility. The same digital chemistry framework supports:
- Full crude oil systems, when global behavior matters
(phase stability, aggregation, interfacial properties, flow behavior) - Targeted chemical subsystems, when the focus shifts to:
- Asphaltenes and resins
- Surfactants and additives
- Solvents and demulsifiers
- Lubricants and specialty chemicals derived from crude fractions
This is particularly important for organizations that operate beyond extraction, where crude oil is also a feedstock for chemical production. Digital models can be refined to focus on the molecular families that matter for performance, stability, or manufacturability – without rebuilding the system from scratch.
Asphaltenes: From problem management to design variable
Asphaltenes remain one of the most expensive challenges in oil and gas operations. Their aggregation behavior impacts flow assurance, processing, and long‑term operability, that said, they are notoriously difficult to characterize experimentally.
With multiscale simulation in Simcenter Culgi, asphaltenes are no longer treated as a dark box. Digital crude oil models enable engineers to:
- Compare aggregation tendencies across crude compositions
- Study the impact of processing history and solvent environment
- Analyze interactions with additives at a molecular level
More importantly, asphaltenes become a design variable, not just a problem to mitigate. Digital chemistry opens the door to:
- Rational screening of inhibitors and dispersants
- Evaluation of processing strategies before deployment
- Exploration of alternative valorization pathways (e.g., materials, additives)
Design exploration first: Screening beats trial and error
Historically, many digital chemistry workflows in oil and gas were designed as one‑off studies, often based on methods and assumptions developed several years ago. That legacy approach tends to:
- Focus on single formulations
- Emphasize validation over exploration
- Underuse automation and design space exploration
Modern workflows shift the paradigm: screen first, refine later.
With Simcenter Culgi, formulation design becomes a screening problem:
- Hundreds of compositions explored virtually
- Key performance indicators computed consistently
- Poor candidates eliminated early, before synthesis or lab testing
Petronas and other operators have demonstrated how digital crude oil models can be used to screen formulation families, rather than optimize a single recipe. See how Petronas decreased formulation development by 85% using Simcenter Culgi. This approach dramatically reduces experimental load while increasing confidence in the final candidates.
From digital chemistry to automated design with HEEDS
The real acceleration happens when digital crude oil models are connected to automated design exploration.
By coupling Simcenter Culgi with HEEDS, organizations can:
- Explore large formulation design spaces automatically
- Optimize multiple objectives simultaneously (performance, robustness, cost)
- Identify non‑intuitive solutions that manual tuning would miss
This combination transforms digital chemistry from a simulation tool into a decision engine, capable of guiding R&D and operational choices at scale.
Why does digital chemistry matter now?
Some earlier digital chemistry narratives in oil and gas were built on workflows developed 4–5 years ago, when automation was limited and models were often static. Today, the landscape has changed:
- Coarse‑grained methods are more mature
- Automation and AI‑assisted exploration are operational
- Integration across simulation, optimization and data workflows is practical
The focus is no longer on proving that digital chemistry works. It is about using it systematically to explore, screen, and design better systems faster.
Digital crude oil as a strategic asset
Digital crude oil models are no longer academic constructs or isolated studies. When implemented in Simcenter Culgi, they become:
- Reusable
- Adaptable
- Scalable across applications
- Directly connected to design exploration workflows
Whether the goal is optimizing production, mitigating risks, or designing new chemical products derived from crude oil, digital chemistry provides a competitive advantage, not by replacing experiments, but by ensuring that only the right experiments are performed.
Ready to learn more about digital chemistry?
Simcenter Culgi offers a versatile, dynamic platform to simulate the most complex systems, faster. Explore this topic further on the Simcenter Culgi website.