{"id":748,"date":"2010-02-22T11:51:22","date_gmt":"2010-02-22T10:51:22","guid":{"rendered":"https:\/\/blogs.mentor.com\/colinwalls\/?p=748"},"modified":"2026-03-26T16:31:55","modified_gmt":"2026-03-26T20:31:55","slug":"staying-in-line","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/embedded-software\/2010\/02\/22\/staying-in-line\/","title":{"rendered":"Staying in line"},"content":{"rendered":"<p>The idea of inlining code &#8211; placing the actual code of a small function at each call site &#8211; is a well known compiler optimization, which I have discussed before. This technique can provide significant performance improvements, due to the elimination of the call\/return sequence. Also, stack usage is reduced. There is a possible cost in terms of increased program memory requirement.<\/p>\n<p>It is reasonable to expect a good C or C++ compiler, when told to compile for speed, to perform inlining automatically. Some C compilers have extensions to give more control over this, but C++ has intrinsic support for inlining within the language &#8230;<!--more--><\/p>\n<p>C++ has a number of keywords that are additional to those in C. Among those is <strong>inline<\/strong>. This is a directive to the compiler requesting that the function is inlined. The compiler is at liberty to ignore the request, if the function is too big or inlining conflicts with optimization settings [i.e. if switches request small code instead of fast code]. The <strong>inline<\/strong> keyword is also implemented in many modern C compilers, as  a language extension, and works in the same way.<\/p>\n<p>But C++ has some other inlining tricks. It is very common for functions, which are part of objects [class member functions] to be small and called with great frequency. Thus, such functions are strong contenders for inlining. They may be declared inline in the same way, using the keyword. However, there is another way to convey the inlining request to the compiler: place the actual code inside the class definition, instead of just declaring the function and defining it outside.<\/p>\n<p>So, C++ has two different ways to declare a function to be inline:<\/p>\n<pre>\tclass T1\n\t{\n\tpublic:\n\t\tvoid foo() \n\t\t{\n\t\t}\n\t};\n\n\tclass T2\n\t{\n\tpublic:\n\t\tvoid foo();\n\t};\n\n\tinline void T2::foo()\n\t{\n\t}<\/pre>\n<p>In this code, both classes have an inline function called <strong>foo()<\/strong>.<\/p>\n<p>This begs a question: what is the difference, in terms of generated code, between these two ways to declare an inline?<br \/>\nPlease post answers as comments or by <a href=\"mailto:colin_walls@mentor.com\">email<\/a>. Sorry, there is no prize, but I will post the result as a comment in a week or so.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>The idea of inlining code &#8211; placing the actual code of a small function at each call site &#8211; is&#8230;<\/p>\n","protected":false},"author":71677,"featured_media":0,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[1],"tags":[313,300,356,327,340],"industry":[],"product":[],"coauthors":[],"class_list":["post-748","post","type-post","status-publish","format-standard","hentry","category-news","tag-c","tag-embedded-software","tag-inline","tag-optimization","tag-programming-languages"],"_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/posts\/748","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/users\/71677"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/comments?post=748"}],"version-history":[{"count":1,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/posts\/748\/revisions"}],"predecessor-version":[{"id":9832,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/posts\/748\/revisions\/9832"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/media?parent=748"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/categories?post=748"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/tags?post=748"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/industry?post=748"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/product?post=748"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/embedded-software\/wp-json\/wp\/v2\/coauthors?post=748"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}