{"id":238,"date":"2020-06-24T10:05:31","date_gmt":"2020-06-24T14:05:31","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/ee-systems\/?p=238"},"modified":"2026-03-26T13:39:33","modified_gmt":"2026-03-26T17:39:33","slug":"modeling-the-true-cost-of-a-wire-harness","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/ee-systems\/2020\/06\/24\/modeling-the-true-cost-of-a-wire-harness\/","title":{"rendered":"Modeling the true cost of a wire harness"},"content":{"rendered":"\n<p>An automotive wire harness rarely has just a single part number that can be ordered and installed in a vehicle. Typically, there are many different versions of the same harness based on the orderable content in the vehicle (figure 1). These versions, often called harness levels, will each have a unique part number. The quantity of these levels and their content is what is typically called complexity. This complexity has a significant impact on the cost of the harness.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"125\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1-1024x125.png\" alt=\"\" class=\"wp-image-241\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1-1024x125.png 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1-300x37.png 300w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1-768x94.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1-1110x136.png 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure1.png 1146w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption>Figure 1: The same harness may have several different versions to support a range of optional vehicle features. <\/figcaption><\/figure>\n\n\n\n<p>Quantifying these costs is often very difficult, especially\nwith manual methods of deriving and costing the complexity solution. Therefore,\ntraditionally, consideration of these complexity related costs has been with\noverly simplified cost modeling techniques. <\/p>\n\n\n\n<h4 class=\"wp-block-heading\">The State of the Art<\/h4>\n\n\n\n<p>It\u2019s not uncommon for organizations to have existing\nrules-of-thumb as a means of trying to capture these costs. For example, an\norganization might simply state that every new part number (harness level)\nequates to some standard cost (ex: $25k). This method is certainly better than\nnot considering complexity related costs at all, and historically has been\n\u2018good enough\u2019.<\/p>\n\n\n\n<p>Today, many automotive OEMs and Tier Ones are struggling\nwith very thin margins and are looking to take pennies out of the material cost\nof the vehicle. In this kind of an environment, over-simplifications and\nrules-of-thumb just aren\u2019t \u2018good enough\u2019. Without proper incentives, designs\nwill be suboptimal and money will be wasted.<\/p>\n\n\n\n<p>Some judgment is required to create models that are simple\nenough to be understood while capturing enough detail to guide engineers to\ncorrect decisions. The reality is that there are thousands of variables that\nslightly affect the cost of designing, manufacturing and shipping a harness.\nThe prevailing ocean currents might affect the amount of fuel required for an\nocean freighter to cross the Pacific. But, is such an unchanging and\ninsignificant variable likely to cause one complexity solution to be more\noptimal than another? If not, it is probably safe to ignore it in the model.<\/p>\n\n\n\n<p>Complexity related costs are particularly difficult to\nquantify since they\u2019re often transparent to organizations and are absorbed in\nthings such as logistics, plant down time, part scrap, etc. It is ultimately up\nto each organization to determine the level of detail that should be captured\nand modeled for their business realities with the ultimate goal of enabling\noptimal design decisions. <\/p>\n\n\n\n<h4 class=\"wp-block-heading\">Piece Cost versus Complexity Management Cost<\/h4>\n\n\n\n<p>Wire harness manufacturers have a very good understanding of what it costs to assemble a wire harness. This piece cost includes the raw materials from the various tier two suppliers, the labor associated with manipulating and assembling these raw materials, the logistics for storing and shipping a single finished product and so on. The piece cost of the wire harness is generally inversely related to the number of harness levels (figure 2). In other words, as the complexity solution reduces the number of levels, the costs go up, while additional levels reduces the piece cost.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure3.png\" alt=\"\" class=\"wp-image-242\" width=\"573\" height=\"597\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure3.png 722w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Modeling-Optimizing-Cost-Variation_WP_Figure3-288x300.png 288w\" sizes=\"auto, (max-width: 573px) 100vw, 573px\" \/><figcaption>Figure 2: The piece cost of a wire harness is inversely related to the number of harness levels. <\/figcaption><\/figure>\n\n\n\n<p>There are additional costs, however, that are not captured in the piece cost that increase with additional levels (figure 3). These are called Complexity Management Costs. By definition, these are costs that are directly related to the number of levels. As a short example, the more levels required for a harness, the more inventory that must be kept on hand. Additional inventory equates to additional costs. As mentioned, it&#8217;s these costs that are difficult to quantify and are often ignored or simply estimated with rule-of-thumb calculations which typically just aren\u2019t good enough.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-983x1024.png\" alt=\"\" class=\"wp-image-240\" width=\"573\" height=\"597\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-983x1024.png 983w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-288x300.png 288w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-768x800.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-1474x1536.png 1474w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4-1110x1157.png 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure4.png 1877w\" sizes=\"auto, (max-width: 573px) 100vw, 573px\" \/><figcaption>Figure 3: Complexity management costs, not captured by the piece cost of a harness, increase with additional harness levels.<\/figcaption><\/figure>\n\n\n\n<p>The true cost of a wire harness is the summation of these two curves, called the Complete Cost Model (figure 4). The ideal complexity solution is the one that is at a minimum spot on the combined cost curve. Without adequately modeling this combined cost curve, it is impossible for a human or an algorithm to arrive at this minimum point except by pure chance.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large is-resized\"><img loading=\"lazy\" decoding=\"async\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-983x1024.png\" alt=\"\" class=\"wp-image-239\" width=\"573\" height=\"597\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-983x1024.png 983w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-288x300.png 288w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-768x800.png 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-1474x1536.png 1474w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3-1110x1157.png 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/Figure3.png 1877w\" sizes=\"auto, (max-width: 573px) 100vw, 573px\" \/><figcaption>Figure 4: The complete cost model (shown in red) represents the true cost of a wire harness.<\/figcaption><\/figure>\n\n\n\n<p>Considering the impact of variation complexity on the overall\ncosts absorbed by the organization is less daunting than one might initially\nthink. Cost models need only be good enough to make correct decisions. To learn\nmore about defining and modeling the various factors that affect the cost of a\nharness, please read our whitepaper <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/topic\/harness-variation-complexity\/63376\" target=\"_blank\" rel=\"noopener\">Modeling\nand Optimizing Wire Harness Costs for Variation Complexity<\/a>. This paper\nincludes a number of real world examples of such costs, a methodology for\ndefining these factors so that they can be modeled, and guidance on methods for\nmodeling them based on how their variability affects overall costs.<\/p>\n\n\n\n<p>Historically, automotive companies have focused on\nunderstanding the piece costs of a wire harness and in many cases largely\nignored the impact of variation complexity on the overall costs absorbed by the\norganization. With vehicles becoming more complex than ever, these methods will\nnot suffice moving forward.<\/p>\n","protected":false},"excerpt":{"rendered":"<p>An automotive wire harness rarely has just a single part number that can be ordered and installed in a vehicle&#8230;.<\/p>\n","protected":false},"author":69444,"featured_media":250,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[85],"tags":[126,124,125,127],"industry":[42],"product":[176],"coauthors":[],"class_list":["post-238","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-ebook","tag-wire-harness","tag-wire-harness-design","tag-wire-harness-engineering","tag-wire-harness-manufacturing","industry-automotive-transportation","product-capital"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/04\/shutterstock_1328952605Heatherpic.jpg","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/238","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/users\/69444"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/comments?post=238"}],"version-history":[{"count":5,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/238\/revisions"}],"predecessor-version":[{"id":382,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/238\/revisions\/382"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/media\/250"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/media?parent=238"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/categories?post=238"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/tags?post=238"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/industry?post=238"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/product?post=238"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/coauthors?post=238"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}