{"id":17,"date":"2020-02-07T15:43:49","date_gmt":"2020-02-07T20:43:49","guid":{"rendered":"https:\/\/blogs.sw.siemens.com\/ee-systems\/?p=17"},"modified":"2026-03-26T13:39:15","modified_gmt":"2026-03-26T17:39:15","slug":"reduce-aircraft-program-risk-with-multi-domain-collaboration","status":"publish","type":"post","link":"https:\/\/blogs.sw.siemens.com\/ee-systems\/2020\/02\/07\/reduce-aircraft-program-risk-with-multi-domain-collaboration\/","title":{"rendered":"Reduce aircraft program risk with multi-domain collaboration"},"content":{"rendered":"\n<p>Electronics and electrical systems are becoming increasingly critical to the operation of modern aircraft. Electronics govern a majority of the critical systems in next generation planes, including flight control actuation, cabin pressurization, and wing de-icing systems. The computers, sensors, and wiring needed to connect and control these systems will come to dominate the interior of the airframe (figure 1). Cabin amenities add even more wiring due to increasing demands for passenger entertainment and communication systems.<\/p>\n\n\n\n<p>Aircraft must also support extensive redundancies to prevent individual system failures from causing catastrophe. The electrical wiring and interconnect systems (EWIS) regulations, set forth by the FAA, outline standards for the design, implementation and maintenance of airplane wiring harnesses. A major component of these regulations is the physical separation and segregation of electrical wires from other systems and from other wiring. This is crucial to achieving safety and redundancy requirements in a plane, and helps prevent failures such as harness chafing, arcing, and electromagnetic interference from damaging or disrupting other systems.<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"678\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-1024x678.jpg\" alt=\"\" class=\"wp-image-18\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-1024x678.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-300x199.jpg 300w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-768x509.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-1536x1017.jpg 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-2048x1357.jpg 2048w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-1-lots-of-wire-small-1110x735.jpg 1110w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption>Figure 1: Electronic devices and electrical systems already take up a large amount of space within the airframe. <\/figcaption><\/figure>\n\n\n\n<p>Despite its difficulty, aerospace design and development\nmust adhere to strict schedules. Delays in progress can cost the company\nmillions of dollars in extra development and follow-on effects of late entry\ninto service. What\u2019s more, errors in design can snowball into larger problems\nwhen manufacturing begins, further jeopardizing progress. Even small inaccuracies\nin wire lengths or spacing between bundles can prevent the proper installation\nof the wire harnesses. This not only adds significant cost but also can delay\ndelivery of aircraft to customers, affecting the company\u2019s reputation and stock\nprice.<\/p>\n\n\n\n<h4 class=\"wp-block-heading\">Facilitating collaboration through ECAD\/MCAD co-design and data exchange<\/h4>\n\n\n\n<p>There is immense pressure on aircraft design teams to move\nquickly and hit program milestones. This can erode the motivation to perform\nextra analysis and validation of aircraft designs before release to initial production.\nChanges that are made without proper communication between the electrical and\nmechanical domains can inadvertently introduce EWIS violations into the design.\nIf these go undetected until critical design review, the manufacturer will need\nweeks or even months to re-design, re-verify, re-release, and then retrofit\neach plane under construction. Such mistakes are incredibly costly and can put\nprograms, careers, and even companies at risk.<\/p>\n\n\n\n<p>Facilitating collaboration among the electrical and\nmechanical engineering domains will be a crucial strategy to avoiding such\ncostly issues moving forward. The optimal strategy is to use a process that\nallows for the incremental and digital exchange of ECAD and MCAD design data\nthroughout the design process. Incremental data exchange ensures that the\nrelevant multi-disciplinary features in the ECAD and MCAD platform\nrepresentations are synchronized at each point in the design. This continual synchronization\ncreates a steady line of communication between the electrical and mechanical\nengineers, increasing productivity and reducing design errors. <\/p>\n\n\n\n<p>Previous efforts to collaborate have met with limited\nsuccess. Earlier ECAD-MCAD collaboration attempts used everything from sticky\nnotes and email, to spreadsheets. These approaches fell far short. As a result,\nmany aerospace development teams resorted to internally developed software and\nprocesses for collaboration that they had to test and verify with each new\nrelease of the underlying ECAD and MCAD tool suites. These locally developed\nsoftware and processes were costly to maintain and required dedicated in-house\nsupport.<\/p>\n\n\n\n<p>The electrical and mechanical design processes can be more connected and collaborative than they are today. Integrated portfolios of engineering software, such as <a href=\"https:\/\/www.sw.siemens.com\/portfolio\/\" target=\"_blank\" rel=\"noopener\">Xcelerator<\/a>, provide these connections between various engineering environments. Seamless cross probing between the two domains enables closer integration and collaboration by enabling the engineers in each domain to design with contextual information from the other.<\/p>\n\n\n\n<p>A key feature of such integration is replacing the\ncumbersome file-based exchange of previous methods. Integration used to depend\non exporting a massive file of changes into a file system for other engineers\nto retrieve and import. Modern electrical and mechanical engineering solutions\ncan integrate at a much deeper level. Capital and NX, for example, support API\nlevel integration, where the solutions connect directly to update the design with\nchanges or new information from each domain. Engineers no longer swap files but\ntruly integrate at the data level via a robust mechanism. <\/p>\n\n\n\n<p>With this integration, design of the electrical system and wiring harness takes place with explicit knowledge of hazardous areas, such as severe weather and moisture prone (SWAMP) areas. Doing so allows the ECAD designer to account for the impact on the electrical performance of these areas when designing the electrical system. On the mechanical side, space reservations can be made and the severity of bends in the harness can be adjusted to account for the wiring bundles that must route through the mechanical structures. With access to this contextual information from other domains, both electrical and mechanical engineers can quickly reconcile incompatibilities between the ECAD and MCAD designs (figure 2).<\/p>\n\n\n\n<figure class=\"wp-block-image size-large\"><img loading=\"lazy\" decoding=\"async\" width=\"1024\" height=\"576\" src=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-1024x576.jpg\" alt=\"\" class=\"wp-image-19\" srcset=\"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-1024x576.jpg 1024w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-300x169.jpg 300w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-768x432.jpg 768w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-1536x864.jpg 1536w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen-1110x624.jpg 1110w, https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/Fig-2-splitscreen.jpg 1920w\" sizes=\"auto, (max-width: 1024px) 100vw, 1024px\" \/><figcaption>Figure 2: Robust integrations allow electrical and mechanical engineers to collaborate more effectively by leveraging contextual information from each domain, and automating change management. <\/figcaption><\/figure>\n\n\n\n<p>Modern electrical systems engineering solutions, such as Capital (part of the Xcelerator portfolio), can also automatically integrate design changes from multiple domains with a high degree of control by the engineer. Engineers can review changes individually, using live cross-probing between electrical and mechanical tools, and accept or reject each change individually (also shown in figure 2). Electrical engineers can also preview the result of a set of changes in a 3D, orthogonal, or unfolding flattened diagram. Furthermore, ownership over data is determined in a granular fashion so that the change policy can be tailored to individual design flows. The pieces available for selection are highly detailed, such that rules may be set for specific attributes of individual components. <\/p>\n\n\n\n<h4 class=\"wp-block-heading\">On time and on budget<\/h4>\n\n\n\n<p>Technological advancements and new market demands have\ncontributed to the exponential rise in the complexity of aircraft designs over\nthe last decade. ECAD-MCAD automated co-design leads to increased productivity while\nensuring a robust design and reducing the cost of quality. Aerospace mechanical\nand electrical designers are now able to synchronize their data more\nefficiently and collaborate more effectively on critical design items, thereby\nensuring proper implementation of design intent. <\/p>\n\n\n\n<p>During design, seamless cross-probing between the electrical and mechanical environments helps designers understand their counterpart\u2019s domain and provides ongoing cross-domain decision assessment. This enables inconsistencies to be identified and resolved early, reducing costly design iterations. ECAD-MCAD co-design, with rich change management support, provides a key enabler for design teams to reach program milestones, ensuring the project proceeds on schedule, while minimizing cost.<\/p>\n\n\n\n<p>To learn more, please read our whitepaper <a href=\"https:\/\/www.plm.automation.siemens.com\/global\/en\/topic\/ecad-mcad-integration\/67550\" target=\"_blank\" rel=\"noopener\">Applying ECAD MCAD Integration to Reduce Program Risk<\/a>. <\/p>\n","protected":false},"excerpt":{"rendered":"<p>Electronics and electrical systems are becoming increasingly critical to the operation of modern aircraft. Electronics govern a majority of the&#8230;<\/p>\n","protected":false},"author":69466,"featured_media":21,"comment_status":"open","ping_status":"open","sticky":false,"template":"","format":"standard","meta":{"spanish_translation":"","french_translation":"","german_translation":"","italian_translation":"","polish_translation":"","japanese_translation":"","chinese_translation":"","footnotes":""},"categories":[85],"tags":[115,113],"industry":[35,39,37,38],"product":[],"coauthors":[],"class_list":["post-17","post","type-post","status-publish","format-standard","has-post-thumbnail","hentry","category-ebook","tag-collaboration","tag-today-meets-tomorrow","industry-aerospace-defense","industry-aerospace-defense-agencies","industry-aircraft-airframes","industry-avionics-defense-electronics"],"featured_image_url":"https:\/\/blogs.sw.siemens.com\/wp-content\/uploads\/sites\/24\/2020\/02\/header-scaled.jpg","_links":{"self":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/17","targetHints":{"allow":["GET"]}}],"collection":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts"}],"about":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/types\/post"}],"author":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/users\/69466"}],"replies":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/comments?post=17"}],"version-history":[{"count":3,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/17\/revisions"}],"predecessor-version":[{"id":23,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/posts\/17\/revisions\/23"}],"wp:featuredmedia":[{"embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/media\/21"}],"wp:attachment":[{"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/media?parent=17"}],"wp:term":[{"taxonomy":"category","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/categories?post=17"},{"taxonomy":"post_tag","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/tags?post=17"},{"taxonomy":"industry","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/industry?post=17"},{"taxonomy":"product","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/product?post=17"},{"taxonomy":"author","embeddable":true,"href":"https:\/\/blogs.sw.siemens.com\/ee-systems\/wp-json\/wp\/v2\/coauthors?post=17"}],"curies":[{"name":"wp","href":"https:\/\/api.w.org\/{rel}","templated":true}]}}