Industries

The role of connectivity in software-defined vehicles

Unlike traditional vehicles, software-defined vehicles (SDVs) are designed to be fully connected. They interact with external systems, gather data from the environment, and stay in sync with cloud services. This high level of connectivity allows SDVs to receive over-the-air (OTA) updates, access real-time traffic and road information, and even predict maintenance needs—all through the power of data. 

The shift to Software-Defined Vehicles is rapidly transforming the automotive industry. Traditional manufacturers following a serial process—developing hardware first and then software—face significant challenges with disconnected departments, teams, and suppliers. This fragmented approach can result in integration issues, extended development cycles, and problems that may only surface after vehicles are on the market.   

Connectivity is the backbone of the SDV, enabling constant communication with the world around it. This communication fuels an array of new capabilities, from personalizing the driving experience to enhancing safety features through Siemens’ automotive solutions. As a result, SDVs are positioned to create a seamless, intuitive experience that adapts to the driver’s needs. 

1. Predictive maintenance: staying ahead of vehicle issues 

Real-time data plays a central role in how software-defined vehicles improve the driving experience. By continuously collecting, processing, and acting on live data, SDVs can respond to changing conditions, anticipate driver needs, and deliver proactive services that increase safety, reliability, and convenience. 

One of the most valuable ways SDVs enhance the driving experience is through predictive maintenance. Rather than relying on fixed service intervals, SDVs use real-time data from onboard sensors to evaluate the health of critical vehicle systems and anticipate maintenance needs before problems occur. 

How predictive maintenance works in SDVs: 

  • Sensor monitoring: SDVs continuously track components such as the engine, brakes, and battery using embedded sensors. These sensors monitor temperature, wear levels, and performance indicators in real time. 
  • Data analysis: The vehicle analyzes incoming data to identify early signs of wear or potential failure. For example, irregular braking performance can be detected long before it affects safety or drivability. 
  • Automated alerts: When potential issues are identified, the vehicle notifies the driver and may recommend or schedule service. This proactive approach helps avoid unexpected breakdowns, reduces repair costs, and extends vehicle lifespan. 

By identifying issues early and keeping drivers informed, predictive maintenance helps ensure SDVs remain dependable, safe, and efficient, contributing directly to a smoother and more confident driving experience. ensures that SDVs remain reliable, safe, and cost-effective. 

2. Personalized settings: tailoring the driving experience 

SDVs provide an unprecedented level of personalization, using real-time data and driver preferences to create a tailored driving experience. This personalization extends beyond seat positioning and mirrors—it includes everything from climate control to route preferences and entertainment options. 

Examples of personalized features in SDVs: 

  • Driver profiles: SDVs can store multiple driver profiles, each with unique settings for seat position, climate control, music preferences, and more. When a driver enters the vehicle, it automatically adjusts to their preferences, creating a familiar and comfortable environment. 
  • Adaptive driving modes: Based on the driver’s habits or the type of journey, SDVs can adjust performance settings. For example, a driver might prefer a more fuel-efficient mode for city driving but opt for a sportier mode on highways. 
  • Voice recognition and natural language processing: By recognizing voice commands and responding to natural language, SDVs offer hands-free control over a range of features, making interactions more intuitive and safer. 

With personalized settings, SDVs turn the vehicle into a space that feels uniquely suited to each driver, enhancing both comfort and convenience. 

3. Connected services: enabling a new ecosystem of features 

Connectivity allows SDVs to access a suite of connected services that go far beyond what traditional vehicles can offer. From infotainment and navigation to real-time weather and location-based services, SDVs provide drivers with a wealth of information and features that make driving more enjoyable and efficient. 

Key connected services in SDVs: 

  • Real-time navigation and traffic updates: By connecting to cloud-based navigation systems, SDVs can provide real-time traffic updates, suggest optimal routes, and adjust for road conditions. This capability helps drivers avoid traffic, save time, and reduce fuel consumption. 
  • In-car entertainment and streaming: SDVs offer access to streaming services, podcasts, and music through integrated infotainment systems. By connecting to mobile networks, drivers and passengers can enjoy on-demand content during the drive. 
  • Location-based recommendations: SDVs can provide recommendations for nearby services based on location and driver preferences. For example, the vehicle might suggest nearby charging stations for electric SDVs or recommend restaurants along the route. 

Through connected services, SDVs create a dynamic, interactive driving experience that meets the needs of modern drivers who expect constant connectivity and access to digital resources. 

4. The role of next-gen connectivity: 5G and V2X communication 

To deliver these real-time, data-driven experiences, SDVs rely on next-generation connectivity solutions such as 5G and Vehicle-to-Everything (V2X) communication. These technologies enable faster data transmission, reduced latency, and increased reliability, which are essential for features like autonomous driving and real-time navigation. 

5G and its impact on SDVs 

With high-speed, low-latency connectivity, 5G enables SDVs to process and share data in milliseconds. This capability is particularly valuable for autonomous driving, where real-time data and instant communication with nearby vehicles and infrastructure are essential for safety. 

Benefits of 5G for SDVs: 

  • Faster response times: 5G enables SDVs to process data almost instantly, which is critical for collision avoidance and adaptive driving functions. 
  • Increased data bandwidth: With more bandwidth, SDVs can handle complex, data-intensive applications, such as high-definition mapping and real-time video processing. 

Vehicle-to-everything (V2X) communication 

V2X is a technology that allows SDVs to communicate with other vehicles, infrastructure, and the cloud, creating an interconnected ecosystem that enhances safety and efficiency. 

V2X applications in SDVs: 

  • Vehicle-to-infrastructure (V2I): SDVs can communicate with traffic lights, road signs, and other infrastructure to receive real-time updates on traffic signals, road conditions, and construction zones. 

By integrating 5G and V2X, SDVs create a safer, more efficient driving environment where vehicles work together to optimize traffic flow and reduce the likelihood of accidents. 

5. The power of digital twin technology in SDV development 

Digital twin technology is revolutionizing how SDVs are developed and maintained. Siemens’ comprehensive digital twin framework enables manufacturers to: 

  • Simulate and validate designs earlier in the development process through Simcenter 
  • Develop hardware and software in parallel rather than sequentially 
  • Reduce development time, costs, and inefficiencies 
  • Enable continuous improvement of software and OTA updates 

The framework supports continuous virtual verification and validation through various testing methods using Siemens’ validation solutions: 

  • Software in the loop 
  • Virtual hardware in the loop 
  • Model in the loop testing 
  • Mixed fidelity models for testing software features against physical systems 

6. Why Siemens software? Powering the future of connected and data-driven vehicles 

As SDVs become increasingly connected and data-driven, Siemens software offers a comprehensive, cloud-based Software-Defined Vehicle framework that leverages Product Lifecycle Management (PLM) and Application Lifecycle Management (ALM) to: 

  • Provide end-to-end lifecycle management 
  • Enable seamless collaboration between suppliers and partners 
  • Allow creation of virtual models for early issue identification 
  • Support remote software commissioning with integrated systems 

1. Robust data management and analytics 

Siemens software provides powerful data management and analytics tools that help automakers collect, process, and analyze real-time data from SDVs. This capability enables predictive maintenance, adaptive settings, and seamless connected services, ensuring that vehicles remain responsive and reliable. With Siemens’ solutions, manufacturers can harness real-time data to continually improve the SDV experience and enhance vehicle performance. 

2. Advanced simulation and testing tools 

To deliver a reliable and seamless connected experience, automakers must rigorously test and validate SDV functions. Siemens offers advanced simulation and testing tools that allow manufacturers to assess vehicle systems under various conditions, ensuring that connected features perform accurately and safely. Siemens’ solutions support end-to-end validation, from data processing to connectivity, helping automakers bring high-quality SDVs to market. 

3. Cybersecurity solutions for connected vehicles 

With increased connectivity comes the need for heightened cybersecurity. Siemens Software provides integrated cybersecurity tools that protect SDVs from cyber threats, ensuring the security of real-time data and connected services. Siemens’ approach to cybersecurity includes encryption, intrusion detection, and OTA security, helping automakers safeguard the connected experience for drivers. 

By choosing Siemens Software, automakers gain access to industry-leading technology that supports the full lifecycle of SDV development—from data management and testing to connectivity and cybersecurity. Siemens enables automakers to build SDVs that meet modern expectations for connectivity, personalization, and safety, delivering a truly revolutionary driving experience. 

4. Connected services: Enabling a new ecosystem of features 

Connectivity allows SDVs to access a suite of connected services that go far beyond what traditional vehicles can offer. Before deploying these services, Siemens’ framework ensures rigorous testing through mixed fidelity models, allowing manufacturers to fine-tune software-based features against physical systems. This approach helps validate that all connected services work correctly in real-world conditions. nditions. 

7. Conclusion: The future of driving with connected, real-time SDVs 

Software-Defined Vehicles are transforming the automotive industry, redefining the driving experience through the power of connectivity and real-time data. By offering predictive maintenance, tailored personalization, and a robust ecosystem of connected services, SDVs enhance convenience, safety, and efficiency on the road. Advanced technologies like 5G and V2X communication further enable SDVs to process data instantly, adapt to driver preferences, and contribute to a safer, more integrated transportation system. 

Siemens software stands as a critical partner for automakers navigating this new era of connectivity and data-driven mobility. With comprehensive solutions for data management, high-performance computing, simulation, and cybersecurity, Siemens enables automakers to build reliable, secure, and highly adaptable SDVs. By partnering with Siemens, automakers are equipped to meet the demands of modern drivers and deliver an unparalleled driving experience that leverages the full potential of connected, real-time data. The future of driving is here, and with Siemens Software, it’s more dynamic, personalized, and connected than ever. 

Nand Kochhar

This article first appeared on the Siemens Digital Industries Software blog at https://blogs.sw.siemens.com/automotive-transportation/2026/01/21/the-role-of-connectivity-in-software-defined-vehicles/